Skip to main content
KBumS
Associate II
Jul 17, 2019 7:16 AM UTC
Solved

Look for CAN example for STM32F4

안녕하세요. stm32446re 로 공부하고있는 학�?입니다.

몇가지 질문사항�?� 있어서 여쭤봅니다.

1. can통신�?� 하고�? 하는�?�, can 2.0b를 �?�용한 예제를 혹시 받아 볼 수 있�?�까요?

2. f446re 와 f429zi를 �?�용하여 can 통신후 모터를 �?�리고�? 하는�?�, 모터 예제�?� 받�?� 수 있�?�까요?

  

미리 �?사�?�사 드립니다 ^^

This topic has been closed for replies.
Amel NASRI
Amel NASRIBest answer
ST Technical Moderator
Aug 5, 2019 9:29 AM UTC

Hello,

This is just a firmware example to get started, and it is up to you to customize it with your hardware.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.

5 replies

Amel NASRI
ST Technical Moderator
Jul 17, 2019 10:07 AM UTC

Hello,

Please use English for your inputs.

Thanks,

Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
KBumS
KBumSAuthor
Associate II
Jul 18, 2019 1:19 AM UTC

Hi. I am a student studying with stm32446re.

I have a few questions to ask.

1. I want to communicate with CAN, can I get an example using CAN 2.0B?

2. I want to run motor after CAN communication with f446re and f429zi. Can I get a motor example?

Thank you in advance ^^

Amel NASRI
ST Technical Moderator
Jul 19, 2019 9:51 AM UTC

Hi @KBumS​ ,

You find a CAN example for STM32F44 on the package STM32CubeF4 (under STM32Cube_FW_F4_V1.24.1\Projects\STM32446E_EVAL\Examples\CAN).

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
KBumS
KBumSAuthor
Associate II
Aug 5, 2019 7:00 AM UTC

The board I'm using is NUCLEO-64 and it doesn't matter if I use EVAL?