Skip to main content
bejanissim
Associate II
April 16, 2009
Question

Load bitmap images to Flash

  • April 16, 2009
  • 5 replies
  • 1877 views
Posted on April 16, 2009 at 11:56

Load bitmap images to Flash

    This topic has been closed for replies.

    5 replies

    bejanissim
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:09

    Dear All,

    I'm using the STM3210E-EVAL board.

    I would like to know how to load bitmap files (like the icons shown in the LCD demo application and in the EVAL_Demonstration_Software).

    I already know that there is a utility such as DfUse but don't know how to use it for loading my own bitmaps.

    If there is another way i will be happy to here it.

    If someone realy did it i will be happy to here the solution.

    Thanks.

    Beja

    bejanissim
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:09

    Dear DOMEN ...

    First,Let me thank you for your response.

    After digging a bit i found that the easiest way loading bitmaps into the NOR Flash component, will be through the DFU mechanism supplied by ST.

    For achieving this goal, few steps are needed:

    1. The bitmap (i used xxx.bmp files) file should be saved as

    16-bits per pixel and R5 G6 B5 (Red 5 bits, Green 6 bits, Blue 5 bits).

    Using photoshop is one option for doing that.

    2. Change the extension of the bmp file to bin (xxx.bmp -> xxx.bin).

    3. Use the DFU supplied by ST for downloading the generated dfu file into

    the NOR Flash (as explained in application note 'an0424_USB').

    That it.

    domen2
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:09

    Not quite the solution, just pointers:

    You could use ie. gimp and save image as .c or .h

    Or, for bigger images, export image as raw, flash it to some fixed position, and use that in your program.

    Or maybe I missunderstood it all :p

    mgieroba9
    Associate II
    October 7, 2015
    Posted on October 07, 2015 at 09:03

    Hi bejanissim!  how now get it from memory in main program ? 

    Tesla DeLorean
    Guru
    October 7, 2015
    Posted on October 07, 2015 at 21:37

    This thread is from over six years ago, and went through a crash of the forum in 2011.

    May be you can better state your question.

    The memory in the STM32 is byte addressable. If you put an image in NOR at 0x64000000 you'd just pass that as an address (pointer) to whatever you have that wants to process or handle the image, not materially different from if you have it in RAM or FLASH.

    void *p = (void *)0x64000000; //??

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..