Skip to main content
vitthal muddapur
Associate III
June 9, 2018
Question

LIS2DW12 INT1?

  • June 9, 2018
  • 0 replies
  • 454 views
Posted on June 09, 2018 at 16:51

Hi,

i am working on stm32l071, interfacing with LIS1DW12 i have configured 

1. Write 64h in CTRL1 // Turn on the accelerometer // ODR = 200 Hz, High-Performance

2. Write 04h in CTRL6 // FS 2 g LOW_NOISE enabled

3. Write 20h in CTRL7 // Do not use low-pass filter for 6D, enable interrupts

4. Write 40h in TAP_THS_X // Set 6D threshold (6D_THS[1:0] = 10b = 60 degrees)

5. Write 80h in CTRL4_INT1_PAD_CTRL // 6D interrupt driven to INT1 pin

6. write 10h in CTRL3 

getting satus SIXED register change the direction of 6D

but didn't get interrupt in MCU from INT1 LIS2DW12 

    This topic has been closed for replies.