Skip to main content
KZait.1
Visitor II
June 2, 2023
Question

Linker handles TFlite differently on different boards

I have two boards: STM32L4xx and STM32H7xxQ.

I use cubeAI 8.0.1 and tflite for a project in vision.

Having set all includes and settings, I successfully build and flash my code on the first board.

The second project uses the same include paths (exported from the first project -> imported), and the only differences must be: 1) board 2) USART port 3) CMSIS/Device

However, the same code fails to compile for the second board, resulting in:

undefined reference to `vtable for tflite::MicroErrorReporter'

which looks like a linker issue.

Are there any special instructions for how to debug what is happening, and understand what caused the difference in compilation between the two projects?

This topic has been closed for replies.