LED don't light on Nucleo STM32F411RE
Hi, I'm getting started with the Nucleo STM32F411RE, and the LED don't light !
Here is my main.c :
//*****************************************************************************
////! \file main.c//! \brief main application//! \version 1.0.0.0//! \date $Creat_time$//! \author $Creat_author$//! \copy//!//! Copyright (c) 2014 CooCox. All rights reserved.////! \addtogroup project//! @{//! \addtogroup main//! @{//*****************************************************************************&sharpinclude <stm32f4xx.h>&sharpinclude <system_stm32f4xx.h>&sharpinclude <stm32f4xx_rcc.h>&sharpinclude <stm32f4xx_gpio.h>void Init(void);void Init(void)
{ RCC_DeInit(); GPIO_InitTypeDef GPIO_InitStructure_Led;RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
GPIO_InitStructure_Led.GPIO_Pin = GPIO_Pin_5;
GPIO_InitStructure_Led.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure_Led.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure_Led.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure_Led.GPIO_Speed = GPIO_Speed_50MHz;GPIO_Init(GPIOA, &GPIO_InitStructure_Led);
}int main(void)
{ Init(); //GPIO_WriteBit(GPIOA, GPIO_Pin_5, Bit_SET); GPIO_SetBits(GPIOA, GPIO_Pin_5); while(1) {}
}//! @}//! @}The build is successful, and I can flash the .bin file via ST-Link Utility. But it doesn't work. The LED stays off.
There is no clue which could lead me to a solution, because all the compiling and flashing processing works fine.
Is there something missing in the code ? Something I forgot to configure ?
Thanks for your help !
#gpio #nucleo-f411 #led