Skip to main content
DShub.1
Associate
July 16, 2023
Question

LCD MB1166-A09 and LCD MB1166-A03

  • July 16, 2023
  • 2 replies
  • 2099 views

Hi,

We had an LCD problem with a recently bought board STM32F769I-DISCO, revision MB1166-A09.

Now it's resolved by recompilation with macro "USE_STM32F769I_DISCO_REVB03" entered in project options.

My question now is how can I make it universal, without compilation for different LCD versions.

How can I check in runtime which version LCD  is installed and call the appropriate version of LCD init function,

" NT35510_Init(NT35510_FORMAT_RGB888, orientation);" or

"OTM8009A_Init(OTM8009A_FORMAT_RGB888, orientation);"   ?

Please help us to resolve this issue, we have a lot of applications with our technologies for this board ( A211400002, MB1166 A-03 / A-02 ) and It is very inconvenient to manage the same projects for different types of LCD.

I develop with MDK-ARM µVision.

 Best regards,

Dmitry S.,

Embedded software engineer

Post edited to adhere community guidelines.

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
July 16, 2023

The boards are not licensed for commercial usage.

You'd likely need to decompose the code difference, either to allow for the common compilation for the two screens, or make two independent libraries with a common interface.

If you can probe the video controllers you might be able to auto-detect which is used. Or have some configuration setting, or OTP, which identifies what you're using moving forward.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Pavel A.
July 16, 2023

Our customers use to add a solder bridge or two on spare GPIOs, populate them at the same time when mounting the 'variable' parts.

Or make a post-programming patch in the flash... and so on.