Skip to main content
aymen
Associate III
December 12, 2012
Question

LCD_8bits

  • December 12, 2012
  • 33 replies
  • 3647 views
Posted on December 12, 2012 at 10:09

I am trying to use an LCD HD44780 (2X40) with STM3210C-eval. I want to configure it for 8 bits mode.

#re-inventing-the-wheel
    This topic has been closed for replies.

    33 replies

    Tesla DeLorean
    Guru
    December 12, 2012
    Posted on December 12, 2012 at 13:22

    I am trying to use an LCD HD44780 (2X40) with STM3210C-eval. I want to configure it for 8 bits mode.

    Ok, but aren't there like thousands of example drivers on the internets already?

    As a minimal post here consider:

    A link to a datasheet on your specific panel.

    A schematic or wiring diagram for your specific configuration.

    A link or attachment of the current code.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    aymen
    aymenAuthor
    Associate III
    December 13, 2012
    Posted on December 13, 2012 at 10:49

    I can write data on the LCD with 4bits mode (LCD_4bits from keil), I want to change the mode to 8bits. I need the pins assignements.

    this is the configuration for 4bits_mode:

    /* PINS:

       - DB4 = PC3

       - DB5 = PC2

       - DB6 = PC1

       - DB7 = PC0

       - E   = PC10

       - RW  = PC11

       - RS  = PC12                                                               */

    #define PIN_E                 (   1 << 10)

    #define PIN_RW                (   1 << 11)

    #define PIN_RS                (   1 << 12)

    #define PINS_CTRL             (0x07 << 10)

    #define PINS_DATA             (0x0F <<  0)

    #define PINS_ALL              (PINS_CTRL | PINS_DATA)

    const unsigned int SWAP_DATA[16] = { 0x0, 0x8, 0x4, 0xC, 0x2, 0xA, 0x6, 0xE,

                                         0x1, 0x9, 0x5, 0xD, 0x3, 0xB, 0x7, 0xF};

    /* Enable Clock for peripheral driving LCD pins                               */

    #define LCD_CLOCK_EN         (RCC->APB2ENR |= (1 << 4)); // enable clock for GPIOC

    /* pin E  setting to 0 or 1                                                   */

    #define LCD_E(x)              GPIOC->ODR = (GPIOC->ODR & ~PIN_E)  | (x ? PIN_E : 0);

    /* pin RW setting to 0 or 1                                                   */

    #define LCD_RW(x)             GPIOC->ODR = (GPIOC->ODR & ~PIN_RW) | (x ? PIN_RW : 0);

    /* pin RS setting to 0 or 1                                                   */

    #define LCD_RS(x)             GPIOC->ODR = (GPIOC->ODR & ~PIN_RS) | (x ? PIN_RS : 0);

    /* Reading DATA pins                                                          */

    #define LCD_DATA_IN           SWAP_DATA[(((GPIOC->IDR & PINS_DATA) >> 0) & 0x0F)]

    /* Writing value to DATA pins                                                 */

    #define LCD_DATA_OUT(x)       GPIOC->ODR = (GPIOC->ODR & ~PINS_DATA) | ((SWAP_DATA[x]) << 0);

    /* Setting all pins to output mode                                            */

    #define LCD_ALL_DIR_OUT       GPIOC->CRL = (GPIOC->CRL & 0xFFFF0000) | 0x00003333; \

                                  GPIOC->CRH = (GPIOC->CRH & 0xFFF000FF) | 0x00033300;

     

    /* Setting DATA pins to input mode                                            */

    #define LCD_DATA_DIR_IN       GPIOC->CRL = (GPIOC->CRL & 0xFFFF0000) | 0x00004444;

    /* Setting DATA pins to output mode                                           */

    #define LCD_DATA_DIR_OUT      GPIOC->CRL = (GPIOC->CRL & 0xFFFF0000) | 0x00003333;

    Andrew Neil
    Super User
    December 13, 2012
    Posted on December 13, 2012 at 11:03

    ''I need the pins assignements''

     

    It's your  project - so it's up to you  to assign whatever pins are available/suitable/conventient in your  particular application!

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    aymen
    aymenAuthor
    Associate III
    December 13, 2012
    Posted on December 13, 2012 at 11:20

    I tried but there is no result. i can't write data.

    Andrew Neil
    Super User
    December 13, 2012
    Posted on December 13, 2012 at 12:47

    So you've done some thing(s) wrong - in your hardware, or in your software, or both.

    Time for you to get checking & debugging...

    As clive1 said, there are thousands of example drivers on the internets already!

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Tesla DeLorean
    Guru
    December 13, 2012
    Posted on December 13, 2012 at 15:33

    It would be more effective if you wired up your 8-bit bus with consecutive GPIO pins so that the bus isn't backward like it is for your 4-bit bus.

    Perhaps you should look at your board schematic and figure out what pins are free.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    jj2
    Associate
    December 13, 2012
    Posted on December 13, 2012 at 16:02

    Your reversal of the ''normal order'' of the Lcd D-Bus is curious.  (only makes sense if your board GPIO pinout enabled fortuitous connection - via the ''tortured'' bus)

    Many, many seek & enjoy the 4 GPIO pin savings when using 4 bits.  And you have that working.  For what good reason do you seek to ''kill'' this working system by moving to 8 bits?

    aymen
    aymenAuthor
    Associate III
    December 18, 2012
    Posted on December 18, 2012 at 14:19

    I have à new LCD(phico d-0 94v-0) wich must be configured in 8bits mode in order to write data.

    i try with 4bits mode but no results

    http://www.datasheetarchive.com/LM2780A2C40HN-datasheet.html

    jj2
    Associate
    December 18, 2012
    Posted on December 18, 2012 at 17:57

    ''i try with 4bits mode but no results.''

    ''No results'' as a diagnosis provides almost NO Value!  Your new Lcd almost certainly includes an HD44780/clone control IC - and all of these are 4 or 8 bit compatible!

    Suspect instead that you have an improper contrast voltage (Vo) setting.  If improper - you will not see the pixel field.  It may be that you need some slight negative voltage on this Vo pin - devil in the detail w/in your data sheet.

    aymen
    aymenAuthor
    Associate III
    December 19, 2012
    Posted on December 19, 2012 at 10:40

    I tried 4bits mode.

    if I connect (D4,D5,D6,D7) with 5v, the first line appears black (high contrast)

    if I connect (D4,D5,D6,D7) with GND, the first line appears black (low contrast)

    after lcd_init();

            lcd_clear();

           lcd_print(''hello'');

    there no caracteres printed in the lcd. No change.