Skip to main content
Mbhir.1
Associate
December 30, 2021
Solved

Laser sensor tw10sp not working correctly

hello everyone, am working with the laser sensor tw10sp to mesure distance and interfacing it with UART. It require commands to work. i send the HEX command via UART and it response always with the same HEX number (clearly something wrong).

Any help please !!

0693W00000HqB96QAF.png

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
January 3, 2022

That's the same question you asked on the Arduino forum.

However, the laser module is not a product of STMicroelectronics, even if there is an STM32F030C8T6 on it. Maybe the description on Aliexpress will help you further?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
January 3, 2022

That's the same question you asked on the Arduino forum.

However, the laser module is not a product of STMicroelectronics, even if there is an STM32F030C8T6 on it. Maybe the description on Aliexpress will help you further?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Mbhir.1
Mbhir.1Author
Associate
January 3, 2022

the sensor is communicating with the st board but the same HEX numbers are returning from it undependenly the command sent from the stm32. in the aliexpress description there is no explanation of such error..