Skip to main content
ZJing
Associate III
August 9, 2023
Question

L431 stops working after enabling DAC

  • August 9, 2023
  • 2 replies
  • 1488 views

I am trying to use the onboard DAC to generate a sine signal. The program runs without any problem on the Nucleo L432KC board but it would not work on our PCB with L431. As soon as the DAC is enabled with LL_DAC_Enable(DAC1, LL_DAC_CHANNEL_1); the program would stop running (or at least it appeared to be stopped from debug view) and all the variable values would reset to 0 in live expressions.

See DAC init code:

 

 

static void DAC_Init(void)
{

	LL_DAC_InitTypeDef DAC_InitStruct = {0};

	/* Peripheral clock enable */
	LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_DAC1);

	/** DAC channel OUT1 config
	*/
	DAC_InitStruct.TriggerSource = LL_DAC_TRIG_SOFTWARE;
	DAC_InitStruct.WaveAutoGeneration = LL_DAC_WAVE_AUTO_GENERATION_NONE;
	DAC_InitStruct.OutputBuffer = LL_DAC_OUTPUT_BUFFER_ENABLE;
	DAC_InitStruct.OutputConnection = LL_DAC_OUTPUT_CONNECT_GPIO;
	DAC_InitStruct.OutputMode = LL_DAC_OUTPUT_MODE_NORMAL;
	LL_DAC_Init(DAC1, LL_DAC_CHANNEL_1, &DAC_InitStruct);
	LL_DAC_DisableTrigger(DAC1, LL_DAC_CHANNEL_1);

}

 

 

DAC start code:

 

 

static void Test(void)
{

	if(!Test_flag)
	{
		if(!((READ_BIT(TIM1->CR1, TIM_CR1_CEN) == (TIM_CR1_CEN)) ? 1UL : 0UL))	//Check if counter is enabled
		{
			LL_TIM_SetCounter(TIM1, 0);
			LL_TIM_ClearFlag_UPDATE(TIM1);
			LL_TIM_EnableIT_UPDATE(TIM1);
			LL_TIM_EnableCounter(TIM1);
		}
		LL_DAC_Enable(DAC1, LL_DAC_CHANNEL_1);
	}

}

 

 

TIM1 interrupt function to calculate for new sine output:

 

 

void TIM1_UP_TIM16_IRQHandler(void)
{
	if(LL_TIM_IsActiveFlag_UPDATE(TIM1))
	{

		LL_TIM_ClearFlag_UPDATE(TIM1);
		LL_TIM_DisableCounter(TIM1);
		LL_TIM_SetCounter(TIM1, 0);

		DAC1->DHR12R1 = (0.9428 / Supply_Voltage * sin((double)DAC_Count / 100 * 2 * PI) + 1) * 2048;
		DAC_Count++;

		if(DAC_Count >= 2500)
		{
			//LL_DAC_Disable(DAC1, LL_DAC_CHANNEL_1);
			Test_flag = 0;
			DAC_Count = 0;
		}

		LL_TIM_EnableCounter(TIM1);

	}

}

 

 

 

What could be the cause of this problem?

Any general help/advice would be appreciated!

 

Zhi

This topic has been closed for replies.

2 replies

ST Employee
August 9, 2023

Hello @ZJing

Have you tried another code example using DAC with your current board?

Note: check AN3126: Audio and waveform generation using the DACin STM32 products

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
waclawek.jan
Super User
August 9, 2023

Make sure there's no short on PA4.  You can try a simple program, setting it as a GPIO Out and toggling, while observing using oscilloscope.

JW