Skip to main content
Badam.17
Associate
June 24, 2019
Question

L4 color space clut

  • June 24, 2019
  • 1 reply
  • 634 views

I only need to display around 8 colors in rgb space and if i use L4 color space i can reduce my framebuffer to the point where i can put the entire framebuffer in internal sram. The only problem is i don't understand how to format the clut in L4.

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
June 25, 2019

It's not given explicitly in RM, but I'd be very surprised if L4 wouldn't decode in the same way as L8 except the upper 4 bits being fixed to 0. In other words, the LUT is the same as in L8 mode, except that you need to provide only the first 16 entries.

A bullet-proof way to do this would be to repeat these 16 entries 16 times.

LUT details are given in the DMA2D foreground and background CLUT interface subchapter of the DMA2D chapter in RM.

JW