Skip to main content
R B
Visitor II
November 9, 2017
Question

KSZ8863 RMII Interface and STM32f207 Communication

  • November 9, 2017
  • 1 reply
  • 1290 views
Posted on November 09, 2017 at 20:22

Hello,

I am currently using HAL library to interface my STM32F207 to a KSZ8863 switch using RMII Interface. The clock 25 Mhz provided externally which is then scaled to 50 Mhz to enable the interface. Now, I can read from the KSZ PHY register, i.e: I can read the CHIP ID and the default reset values but writing to the Ethernet PHY register is a complete failure. 

Do I have to implement a bit bash mechanism as mentioned over here? Do I have to initialize both the PHY Ports?

https://community.st.com/0D50X00009XkYftSAF

 

Because I have tried that method and it is unsuccessful. I have pored through the datasheet to no avail. 

Does anyone have a solution or tips on how to proceed?

Thanks and Regards.

#ksz8863
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    August 10, 2018

    Sorry, bumping old zombie unanswered questions off my feed

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..