@Giorgi_Kvernadze wrote:
Is using the alternative pins of FMC_NBL1, that are not physically present on the 144 package, still a possibility?
Like afaik, they are still there on the chip itself, just aren't connected to a physical pin.
It's available internally on the die but not bounded/exposed externally off the chip.
@Giorgi_Kvernadze wrote:
Can I somehow configure to use one of those and route their output to a free GPIO pin?
I don't think it is doable. NBLx are signals managed by the FMC according to the CPU transactions and they are managed automatically by Hardware.
So I suggest to use another package that has NBL1 available outside PA15.
Think about LQFP144 SMPS package where FMC_NBL1 is available also on PB11.
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.