Skip to main content
bardeau tracy
Associate
March 8, 2018
Question

Jitter less than 20ns with STM32L476

  • March 8, 2018
  • 10 replies
  • 3118 views
Posted on March 08, 2018 at 16:28

Hi,

I've a problem with the jitter of my program on STM32L476.

First of all, I'm introduced you my project.

A signal TLL with a frequency of 1KHz to 50 KHz must be multiplied by a sinusoide or square analogique signal (10Hz to 1KHz) like a AM modulation. Then with the DAC of STM32 a results could be send in analogique format.

at the beginning I'm use a DMA for the ADC/DAC and a callback function trig by timer 6 (sampling Time 100 Khz).

In a call back function I'm get the state of the TTL and multiplied by the results of ADC (result *1 if the TTL state was SET or result *-1 if the results state is RESET), then I get the result in the DAC.

When I look the result with an osciloscope I see a 8 µs jitter and the frequency results is so bad especially near 50 Khz. period for 50Khz is 20 µs so sometime I see 35 KHz and sometime 80 KHz.

So I have modified my code like that. I made a new extern interuption on signal TTL and change the state of a variable 1 then -1. I use freeRTOS and give the high priority to the EXTI interupt. In a callback TIMER 6 i use the result of the ADC multiplied by the variable 1 or -1.

When I look the result with an osciloscope I see a 100ns jitter for the EXTI interrupt and always 8 µs jitter for the final results.

 So my question is what is the minimal jitter I could have for my project?

I don't know really freeRTOS and i do'nt understand why i can't get a prioity value less than 5. This is a probem because i want the maximum priority to the EXTI interrupts to reduced the jitter.

Can I do like that:

only one interruption EXTI on signal TTL (between 1 to 50 Khz).

in the function of EXTI :

I manually start the DAC with the value of ADC( The first conversation could be wrong but it doesn't matter)

Then I manually START ADC (one sample)

I change the state of a variable example stateTTL = StateTTL * -1 to change 1 in -1 or -1 in 1.

I multiplied the value of ADC by stateTTL.

I think when I do like that I have the jitter of only the EXTI interrupts + the DAC jitter isn't it?

I want a precison of 50 Hz at 50KHz so I must have a global jitter less than 20ns. It is Possible?

Thank you for your answear.

here i attached a schema

    This topic has been closed for replies.

    10 replies

    Tesla DeLorean
    Guru
    March 8, 2018
    Posted on March 08, 2018 at 17:07

    >>I must have a global jitter less than 20ns. It is Possible?

    Interrupting (at 100 KHz and 50 KHz), calling through a couple of levels of handlers/callbacks, on a machine running at 80 MHz (12.5ns cycle time, perhaps >150ns latency, 50ns bus accesses). I'd be surprised.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    bardeau tracy
    Associate
    March 9, 2018
    Posted on March 09, 2018 at 11:44

    Latency is not my problem, my problem is jitter.

    So if the latency is 1 or more than one Âµs it is not a problem.

    if the latency is one time 1000 ns and other time 1400 ns that it a problem for me (jitter 400 ns)

    I must have a constant latency for my project.

    Tesla DeLorean
    Guru
    March 9, 2018
    Posted on March 09, 2018 at 16:40

    >>I must have a constant latency for my project.

    The responsiveness of the system is going to be non-deterministic.

    >>So my jitter could be only arrived cause of EXTI interrupt priority and Write on the DAC priority.

    Really, so the cache, the flash line width, multi-cycle bus access cycles, bus contention, multi-word load/store, tail-chaining, etc won't impact things?

    The phase alignment of your external clock/signals with respect to internal clock?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    henry.dick
    Associate II
    March 8, 2018
    Posted on March 08, 2018 at 19:22

    '

    I must have a global jitter less than 20ns.'

    then you seemed to have tried all you can to defeat yourself: the use of RTOS, interrupts, multification, ..., will all overwhelm that 20ns requirement.

    if you really want to have low jitter, think of a hardware based solution, like an analog / switched digital solution.

    bardeau tracy
    Associate
    March 9, 2018
    Posted on March 09, 2018 at 12:08

    then you seemed to have tried all you can to defeat yourself: the use of RTOS, interrupts, multification, ..., will all overwhelm that 20ns requirement.

    that why i will try a new solution on monday and give you my result.

    my new solution is to immidatiely after a EXTI interrupt to convert a variable in the DAC.

    keep the minimum interrupt ( only EXTI), I remove DMA timer 6 ... I remove RTOS wich use SYSTICK.

    So my jitter could be only arrived cause of EXTI interrupt priority and Write on the DAC priority.

    Like that I minimise the jitter.

    for example:

    results DAC T0= +30 ns

    results DAC T1= +10ns

    results DAC T2= -10 ns

    results DAC T3= +10 ns

    results DAC T4= +30 ns

    results DAC T5= +50 ns

     it's not a probleme because the frequency do not really change

    I think the real probleme it's the extrem and regularly jitter

    results DAC T0= -20 ns

    results DAC T1= +20 ns

    results DAC T2= +60 ns

    results DAC T3= +100 ns

    results DAC T4= +140 ns

    results DAC T5= +180 ns

    is this case the frequency is regularly different that the frequency i want for example:

    for 40 000HZ TTL I have a result of 39936 KHz.

    other thing it's one time of 100 sample the result have a jitter of 100 ns it's not a problem but i must have the maximum result with the good frequency.

    Jan Waclawek
    Visitor II
    March 9, 2018
    Posted on March 09, 2018 at 18:32

    my new solution is to immidatiely aftera EXTI interrupt

    Forget about EXTI.

    Use timer input capture to timestamp the digital ('TTL') signal's transitions. Set up DAC to be started from a timer's compare event. Sample analog input in regular 100kHz rate, and set up an interrupt triggered by the ADC conversion. In that, check if capture happened, and based on that schedule the next compare event to start DAC - a fixed number of cycles delayed from the capture, or 10us from the last compare if there was no capture - and the required value for DAC. There may be details to be resolved, e.g. to prevent DAC conversion to be scheduled closer together than the conversion duration is.

    JW

    T J
    Senior III
    March 10, 2018
    Posted on March 10, 2018 at 06:45

    I am thinking that the SAI interface would offer clean Jitter free analogue. since that is the primary function of SAI

    I guess that requires extra circuitry.to convert it to an actual analog signal.

    You have 2x SAIs on board this chip...

    I guess you could use one as the analogue receiver and one as the transmitter,

    but your latency may blow out,

    how much latency can you tolerate ?