Skip to main content
ybenharim10
Associate III
August 29, 2009
Question

J-Link error

Posted on August 29, 2009 at 23:43

J-Link error

    This topic has been closed for replies.

    26 replies

    ybenharim10
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:59

    I assume that the problem was caused by a ''bad'' program, that changed the STM configuration in a way that disrupted the JTAG communication (for example: changing the JTAG pins to GPIO configuration).

    I did not added strange features, the program just did not operated normally.

    The second board got sick only after I worked with the bad program.

    jj_it
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:59

    Very well explained - thank you. You diagnosed the problem instantly and resolved it.

    Now I offer a technique to ''recover JTAG'' - WITHOUT having to change the boot pins and having to load a ''safe'' new program. We use this method on all of our STM32 (and other ARM) designs - it has often ''saved'' us.

    Simply include small code which ''looks'' for some special event (switch closure, ADC level, etc.) BEFORE you change (either deliberately or inadvertently) switch JTAG pin/pins to GPIO. Place this code very early in your program - this allows an easy/graceful recovery should you lose JTAG... (in our case - we restore JTAG when ''special'' event occurs. During development - when JTAG use is heavy - we reverse the ''default.'')

    [ This message was edited by: jj.sprague on 20-01-2009 17:58 ]

    jilisegiar
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:59

    When booting from RAM, the ''bad'' code resides in Flash will not be executed. So you can connect to STM32 device. In this case you can use JFlash or program running from RAM to erase the flash or you can load a ''correct'' program into Flash(and not RAM)which will replace the bad one. After this you can boot from Flash.

    jpnorair23
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:59

    I have been revisiting the STM32 hardware recently and I am still unable to use the JLink program to erase. I suspect this might be due to my having old STM32 chips or, more likely, a different board than the standard STM32 kit.

    So I wrote this program to compile and load via IAR. Quick and dirty, but it works in place of JLink's ''erase chip''.

    Code:

    void main ( void ) {

    u32 i;

    u32 start_addr;

    u32 end_addr;

    RCC_DeInit();

    RCC_HCLKConfig(RCC_SYSCLK_Div1);

    RCC_PCLK2Config(RCC_HCLK_Div1);

    RCC_PCLK1Config(RCC_HCLK_Div1);

    RCC_ADCCLKConfig(RCC_PCLK2_Div6);

    RCC_AHBPeriphClockCmd( RCC_AHBPeriph_FLITF, ENABLE);

    RCC_APB1PeriphClockCmd( (RCC_APB1Periph_BKP | RCC_APB1Periph_PWR) , ENABLE);

    FLASH_SetLatency(FLASH_Latency_0);

    FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable);

    FLASH_HalfCycleAccessCmd(FLASH_HalfCycleAccess_Enable);

    /* FLASH_START_ADDR = 0x08000000 on as many STM32 models as I know

    * FLASH_PAGE_SIZE usually is 1024, check your device

    * FLASH_NUM_PAGES depends on your device

    */

    start_addr = FLASH_START_ADDR;

    end_addr = FLASH_START_ADDR + (FLASH_PAGE_SIZE*FLASH_NUM_PAGES);

    FLASH_Unlock();

    for (i=start_addr; i<end_addr; i+=FLASH_PAGE_SIZE) {

    FLASH_ErasePage(i);

    }

    while (1);

    }

    jpnorair23
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:59

    I've been hammered by this problem for a long time, now. It seems to happen to me after exiting a debug session inharmoniously, which is inevitable because even it the ''debug'' mode the STM32 doesn't seem to be haltable when it's in sleep mode.

    Anyway, I'm pretty fed up and I hope that simply using a newer revision will fix this.

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:59

    Hi,

    Have you tried the lasted J-link software here :

    http://www.segger.com/download_jlink_beta.html

    ?

    Cheers,

    STOne-32.