Skip to main content
NTosi
Associate III
April 7, 2025
Question

It is not possible to set RTC output on Tamper pin for Second and Alarm Pulse.

Hi,

 

I try the whole day with an F103C8 to have the Alarm Pulse on Tamper Pin C13 but it is not possible, I tried with PullUp resistor and also I tried to configure manually the GPIO Pin to AF OD config. But with my Osciloscope I cannot see anything. Only works the Clock divided with 64 output, with this configuration I can see the clock with a 511Hz signal. I tried CubeIDE 1.15 and 1.18 with tha same results.

Any Ideas?

 

Kind regards,

Niko

This topic has been closed for replies.

3 replies

ST Employee
April 8, 2025

Hello @NTosi, 

Could you share the RTC configuration that's not working? 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
NTosi
NTosiAuthor
Associate III
April 8, 2025

sure, its with alarm as output but second pulse has also the same problem.

 

Kind regards,

Niko

 

 

NTosi
NTosiAuthor
Associate III
April 10, 2025

@Sarra.S 
Hello, any news from the problem?

 

kind regards,

Niko