Skip to main content
Visitor II
January 13, 2025
Question

Issues with STM32H753VIT6 After Clock Changes - Not Responding or Reprogramming

Moved from the MPUs forum - H7 is an MCU, not MPU


I am a complete beginner with STM32, and I'm currently working on a project where I need to transmit a simple 16-bit ADC value to USB using my STM32H753VIT6. I'm trying to figure out things myself, but I seem to have encountered an issue and could really use some guidance.

Here’s the situation:

  1. When I started the project, all the basic peripherals were running at a 64 MHz clock speed.
  2. To improve performance, I increased the clock speed to 480 MHz for the peripherals that can handle that.
  3. I then adjusted the ADC clock to 100 MHz, and everything seemed to work fine (the IDE supported it without showing any errors).
  4. However, I then changed all clocks to 120 MHz, the ADC clock to 64 MHz, and kept the USB_OTG at 48 MHz (I never changed this one).
  5. After flashing the STM32 with these settings, the device is no longer responding and I cannot reprogram it.

I’m completely new to this, so I’m not sure where I went wrong. Could this be a clock configuration issue? Is there a way to recover the device and reprogram it?

Sorry if I did something foolish, but I’d really appreciate any help or suggestions on how to proceed!

Thanks!

This topic has been closed for replies.

3 replies

ELABI.1
ST Technical Moderator
January 15, 2025

Hi @Arv0032,

You can use the CubeProgrammer to unlock your board by using flash erase. You can refer to the User Manual UM2237 of the CubeProgrammer for more details, specifically section 2.3 Memory programming and erasing.

Do you generate the code with MX or make the modifications manually?

Thank you.

ELABI.1

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
January 15, 2025

If you pull BOOT0 pin HIGH, the chip will start in the System Loader ROM rather than code you have installed. This might provide a window/method to erase your code.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
mƎALLEm
ST Technical Moderator
January 15, 2025

Hello,

To be efficient, need to provide the ioc that generates the working configuration (with 480 MHz I think) and the one (ioc) generating the non-working project (with 120 MHz I think).

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.