Skip to main content
developer2
Senior
October 4, 2013
Question

issue with USB CDC

  • October 4, 2013
  • 0 replies
  • 395 views
Posted on October 04, 2013 at 16:00

Hi All,

i'm using STM32F407, USB Device library V1.1.0 / 19-March-2012,

i'm able to receive from PC to STM bytes using CDC, but i'm unable to send to PC from STM :(

i modified function like this :

static uint16_t VCP_DataTx (uint8_t* Buf, uint32_t Len)

{

  for( uint16_t i = 0; i < Len; i++)

  {

    APP_Rx_Buffer[APP_Rx_ptr_in] = CDCdebug_tx_buf[ i ];

    APP_Rx_ptr_in++;

    /* To avoid buffer overflow */

    if(APP_Rx_ptr_in == APP_RX_DATA_SIZE)

    {

      APP_Rx_ptr_in = 0;

    }

  }

  CDCdebug_tx_buf_len=0;

  return USBD_OK;

}

most of lines was taken from CDC template from Library,

thanks for all replies,

Kind regards,

UPDATE: i forgot to call that function ... it's not called by any Handler as i thought,

please remove topic ...
    This topic has been closed for replies.