Skip to main content
CTabo.1
Senior
February 8, 2024
Solved

Issue with USART RXFIFO threshold configuration

Hello,
I am developing an application on STM32H563 MCU and NUCLEO board.

I have the following problem when trying to configure USART2 RXFIFO threshold.

In particular, on a transmission completed event, inside the ISR, I need to configure the RXFIFO threshold based on the expected number of bytes to receive.
I try to do this, using the LL_USART_SetRXFIFOThreshold(), but I see that it doesn't have effect on the RXFTCFG bits of register CR3, that remains stuck at 0.

What am I doing worng?

Regards,
Carlo

This topic has been closed for replies.
tjaekelBest answer
Lead II
February 10, 2024

Often, you can change the peripheral (device) config only when it is disabled. Disable the USART and change it, enable afterwards again. I do not think it is good idea this stuff inside an ISR.

BTW: FIFO is not related to "expected number of bytes to receive". For instance, if you expect 100 bytes - you cannot configure FIFO for 100 bytes (the FIFO is not so large).

The FIFO is not related to number of transferred bytes: it is there to help FW to relax (to have option when FW is busy N bytes are not lost). Check the FIFO size possible.
BTW: a FIFO can make things also a bit more complicated (e.g. received byte still sitting in FIFO: you have to check on reception if there is still something in FIFO).

Do not use a FIFO as a "receiver buffer": it is there just to make the FW a bit more relaxed, when to read the FIFO.
If you use FIFO as receiver buffer - check the FIFO size (and make sure that transmitter has stopped sending data, otherwise FIFO overflows).

2 replies

tjaekelBest answer
Lead II
February 10, 2024

Often, you can change the peripheral (device) config only when it is disabled. Disable the USART and change it, enable afterwards again. I do not think it is good idea this stuff inside an ISR.

BTW: FIFO is not related to "expected number of bytes to receive". For instance, if you expect 100 bytes - you cannot configure FIFO for 100 bytes (the FIFO is not so large).

The FIFO is not related to number of transferred bytes: it is there to help FW to relax (to have option when FW is busy N bytes are not lost). Check the FIFO size possible.
BTW: a FIFO can make things also a bit more complicated (e.g. received byte still sitting in FIFO: you have to check on reception if there is still something in FIFO).

Do not use a FIFO as a "receiver buffer": it is there just to make the FW a bit more relaxed, when to read the FIFO.
If you use FIFO as receiver buffer - check the FIFO size (and make sure that transmitter has stopped sending data, otherwise FIFO overflows).

CTabo.1
CTabo.1Author
Senior
February 13, 2024

Thank you @tjaekel,

I was used to consider FIFO as "receive buffer", because of my experience with TI DSP, where USART FIFO handling is more flexible.

In that case, indeed, I could modify the deeper FIFO length (16 characters) on the fly, without enabling/disabling USART, setting it to the precise number of characters expected.

Regards,
Carlo