Skip to main content
Karthika ML
Associate
Oct 16, 2017 3:50 AM UTC
Solved

Issue with STM32F107 bootloader. The jump to application fails

Posted on October 16, 2017 at 05:50

Hi, I have got an issue with STM32F107 bootloader. The jump to application fails and results in hardfault. Before jumping, I have disabled all interrupts including systick timer and also set the MSP to the initial value as needed for the application program. Is there anything else to be taken care of, before making the jump? Could someone help? I have just copied the relevant part of my code below.

/********************************* declarations  and defines     ****************************/

unsigned               *p;

void                       (*user_code_entry)(void);

unsigned int          Address_PgrmCounter;

#define                  APPLICATIONADDRESS          (unsigned int)0x800e000

/********************************* reset system and disable all interrupts****************/

HAL_RCC_DeInit(); 

HAL_DeInit();

SysTick->CTRL &= ~0x00000011; /* Disable systick counter*/

__HAL_RCC_TIM2_CLK_DISABLE();

__disable_irq();

for(i=0;i<68;i++)

{

HAL_NVIC_DisableIRQ(i);

}

for(i=0;i<=15;i++)

{

__HAL_GPIO_EXTI_CLEAR_IT(i);

}

SCB->ICSR &= ~(0x10000000) ;

/********************************* set MSP  **********************************************/

__set_MSP(APPLICATIONADDRESS);

/********************************* Jump to application 

********************************/

Address_PgrmCounter = APPLICATIONADDRESS + 4;

p = (unsigned *)(Address_PgrmCounter);

user_code_entry = (void *) *p;

user_code_entry();
    This topic has been closed for replies.
    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Oct 16, 2017 8:19 AM UTC
    Posted on October 16, 2017 at 10:19

    Can we try to not jam the entire question in the title, edit to fix.

    You want the MSP to be a RAM address. Ie the value AT the application address and NOT the application address.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

    3 replies

    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Oct 16, 2017 8:19 AM UTC
    Posted on October 16, 2017 at 10:19

    Can we try to not jam the entire question in the title, edit to fix.

    You want the MSP to be a RAM address. Ie the value AT the application address and NOT the application address.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Karthika ML
    Associate
    Oct 17, 2017 2:37 PM UTC
    Posted on October 17, 2017 at 14:37

    Thanks for the reply. It helped! Jumping to application is successful after rectifying the MSP value.

    Tesla DeLorean
    Guru
    Oct 17, 2017 12:41 PM UTC
    Posted on October 17, 2017 at 14:41

    __disable_irq(); // if you do this you must enable on the other side

    __set_MSP(*((uint32_t *)APPLICATIONADDRESS)); // the content of SP describe IN the vector table

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..