Question
ISSUE with Erase Command of STM32F4 CAN Bool loader
Posted on June 20, 2017 at 22:02
I'm using the CAN Boot loader on the STM32F405xx chip and have an issue with the Erase command (0x43).
I am able to execute 0x00, 0x01, 0x02, 0x11, 0x21 & 0x31 as described in the Protocol Document, however when ID: 0x43 is attempted with Data: 0xFF (Global Erase) parameter or, for example, a 3 page erase with Data: 0x02, 0x00, 0x06 & 0x07
There is no ACK nor a NAK response.
Any ideas? (Boot loader version returned is 2 and ID is 0x0413)