Skip to main content
JP.4
Associate
Sep 6, 2024 8:54 AM UTC
Solved

ISSUE WITH DSI MIPI ADAPTIVE COMMAND MODE HP TRANSMISSION


I am currently working with the STM32U5G9J-DK1 development kit interfacing with a Tianma-based display. I have successfully managed to update the display using adaptive command mode with DSI long and short write commands. However, I am encountering issues related to the refresh rate and switching modes:

  1. Issue with Refresh Rate:
  • While updating the display using long write DSI commands, I observed that the refresh rate is significantly slow. To optimize this, I attempted to change to High-Performance (HP) mode after the initialization commands.
  1. Problem Switching to High-Performance Mode:
  • After the initialization commands and sending a pixel memory write command, I disabled the DSI long write command from low power to check if the display would operate in HP mode.
  • However, when I disable the low power (LP) mode for long write commands, the display shows nothing. The display only works if I enable LP mode for the long write.
  1. Configuration Details:
  • I am using FIFO while writing pixels in long write mode.
  • I have confirmed that the initialization sequence and command settings are correct, as they work in LP mode.
  • The issue arises when attempting to transition from LP mode to HP mode.

Request for Assistance:

Could you provide guidance on:

  • Why the display does not work in HP mode after disabling LP mode for long write commands?
  • Are any additional settings or configurations required to enable proper HP mode operation?

Your assistance in resolving this issue would be greatly appreciated.

Thank you.

Best Regards,

JAYA PRAKASH P

EMBEDDED MODULE LEAD

EMAIL: jayaprakash_p@aktisengineering .com

This topic has been closed for replies.
KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Sep 10, 2024 2:40 PM UTC

Hello @JP.4 ,

 

What do you mean by High-Performance (HP) mode? Do you mean High-speed mode?

For more information about REFRESH Rate and High speed mode, I recommend you to take a look at AN4860: Introduction to DSI host on STM32 MCUs and MPUs 

Could you please share you project?

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

3 replies

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Sep 10, 2024 2:40 PM UTC

Hello @JP.4 ,

 

What do you mean by High-Performance (HP) mode? Do you mean High-speed mode?

For more information about REFRESH Rate and High speed mode, I recommend you to take a look at AN4860: Introduction to DSI host on STM32 MCUs and MPUs 

Could you please share you project?

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
JP.4
JP.4Author
Associate
Oct 17, 2024 7:12 AM UTC

HELLO KDJEM.1

                           

Thank you for the clarification and your assistance with my question. Your input has been constructive, and I appreciate your support. Still, we are working on it once we reach some level we will share the project for more review...

Best regards,

JAYAPRAKASH P

AKTIS ENGINEERING SOLUTION PVT LMT

David George
Associate III
Oct 24, 2025 3:30 PM UTC

Hi JP.4 - did you ever get a fix for your DSI problem? I have exactly the same issue myself - works in LP mode, but not in HS mode.

I scoped the line data in HS mode and the data output is actually different from that I expect, it often misses off the first byte (the ID byte from the Header).