Skip to main content
Deepak Soni
Visitor II
May 24, 2018
Question

Issue with ADRDY of ADC1_ISR register on NUCLEO-H743ZI ADC1

Posted on May 24, 2018 at 10:55

Hi, I am trying to use NUCLEO-H743ZI ADC1, I am following the procedure that is recommended in the reference manual, getting out of deep power down, turning on and waiting for voltage regulator to stablize and then confirming these two things are happening. After this when I set ADEN bit of ADC1->CR register and polling for the ADRDY of  ADC1_ISR register, it is not getting set, means adc is not getting ready. I haven't changed any clock or power setting those are running in post reset default state. I am attaching my whole program with the library I am using, pease help me with this.

Thank You

    This topic has been closed for replies.

    1 reply

    Amel NASRI
    ST Technical Moderator
    June 26, 2018
    Posted on June 26, 2018 at 12:55

    Hi

    Soni.Deepak

    ‌,

    The following ADC examples are available in

    https://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-mcu-packages/stm32cubeh7.html

    package underSTM32Cube_FW_H7_V1.2.0\Projects\STM32H743ZI-Nucleo\Examples\ADC:

    0690X0000060BtaQAE.png

    Select one of them and try it. If the initially described issue is still there, please update us.

    Otherwise, check the differences between your settings and the ones in the selected example to know what is wrong in your case.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.