Skip to main content
Associate III
May 16, 2024
Solved

Issue receiving CAN Frames

Hello ST community,

 

I am currently programming an ECU system, using f446re nucleo board. Right now i am trying to communicate with BMS using CAN communication.

So far, everything has been set: CAN Initialization and start, sending works properly.

The issue i am facing is that i cannot receive frames from battery, even though i can communicate with laptop for UDS protocole (Reception works properly in that case), but when i try with the battery, the debug mode doesn't stop at the rx interrupt routine.

I have verified the CANFilter configuration to make sure, i didn't see any mistake, nothing has been changed but i only can communicate with UDS frames and not with batteries.

for example: frame ID 0x586 entering fifo0 with such a filter:

 

void CAN_Filter_FIFO0(CAN_HandleTypeDef* hcan)

{

CAN_FilterTypeDef canfilterconfig;



canfilterconfig.FilterActivation = CAN_FILTER_ENABLE;

canfilterconfig.FilterBank = 10;

canfilterconfig.FilterFIFOAssignment = CAN_FILTER_FIFO0;

canfilterconfig.FilterIdHigh = 0x580 << 5; // According to the DBC

canfilterconfig.FilterIdLow = 0x0000;

canfilterconfig.FilterMaskIdHigh = 0xfe0<<5;// Calculation of the mask according to the DBC

canfilterconfig.FilterMaskIdLow = 0x0000;

canfilterconfig.FilterMode = CAN_FILTERMODE_IDMASK;

canfilterconfig.FilterScale = CAN_FILTERSCALE_32BIT;

canfilterconfig.SlaveStartFilterBank = 13;

HAL_CAN_ConfigFilter(hcan, &canfilterconfig);

}

Please let me know if anyone has any idea.

This topic has been closed for replies.
Erwan03Best answer
Associate III
May 21, 2024

Alright, found the problem, I was using both fifo0 and fifo1 for receiving whereas i had to use only one for all the frames. Don't know how to use both of them s

void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
	HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &RxHeader, RxFrame);
	 {
		 switch(RxHeader.StdId)
		 {
		 	 case 0x586:
				 BatteryChargeCurrent_rcv(RxFrame, &rx_BCC); //Receive frame
				 BatteryChargeCurrent_memHandler(rx_BCC, &h_BCC); //handle memory
				 BCCFlag++;
				 break;
		 	case 0x591:
				 BatteryCurrentLimit_rcv(RxFrame, &rx_BCL); //Receive frame
				 BatteryCurrentLimit_memHandler(rx_BCL, h_BCL); //handle memory
				 BCLFlag++;
				 break;
			 case 0x587:
				 BatteryStatusCharge_rcv(RxFrame, &rx_BSC); //Receive frame
				 BatteryStatusCharge_memHandler(rx_BSC, h_BSC); //handle memory
				 BSCFlag++;
				 break;
			 case 0x580:
				 BatteryStatusGeneral_rcv(RxFrame, &rx_BSG); //Receive frame
				 BatteryStatusGeneral_memHandler(rx_BSG, h_BSG); //handle memory
				 BSGFlag++;
				 break;
			 case 0x59f:
				 BatteryVehicleHandling_rcv(RxFrame, &rx_BVH); //Receive frame
				 BatteryVehicleHandling_memHandler(rx_BVH, h_BVH); //handle memory
				 BVHFlag++;
				 break;
		 	 case 0x24:
		 		 EPIC_PMZ_A_rcv(RxFrame, &rx_pmzA); //Receive frame
		 		 EPIC_PMZ_A_memHandler(rx_pmzA, h_PMZ_A); //handle memory
		 		 break;
		 	 case 0x50:
		 		 EPIC_PMZ_C_rcv(RxFrame, &rx_pmzC); //Receive frame
		 		 EPIC_PMZ_C_memHandler(rx_pmzC, h_PMZ_C); //handle memory
		 		 break;
		 	 case 0x5A:
		 		 EPIC_PMZ_E_rcv(RxFrame, &rx_pmzE); //Receive frame
		 		 EPIC_PMZ_E_memHandler(rx_pmzE, h_PMZ_E); //handle memory
		 		 break;
		 	 case 0x5E:
		 		 EPIC_PMZ_G_rcv(RxFrame, &rx_pmzG); //Receive frame
		 		 EPIC_PMZ_G_memHandler(rx_pmzG, h_PMZ_G); //handle memory
		 		 break;
		 	 case 0x60:
		 		 EPIC_PMZ_H_rcv(RxFrame, &rx_pmzH); //Receive frame
		 		 EPIC_PMZ_H_memHandler(rx_pmzH, h_PMZ_H); //handle memory
		 		 break;
		 	 case 0x4e2:
		 		 EPIC_PMZ_I_rcv(RxFrame, &rx_pmzI); //Receive frame
		 		 EPIC_PMZ_I_memHandler(rx_pmzI, &h_PMZ_I); //handle memory
		 		 break;
		 	 case 0x621:
		 		 HMI_DATA1_rcv(RxFrame, &rx_cluster); //Receive frame
		 		 HMI_DATA1_memHandler(rx_cluster, h_HMI); //handle memory
		 		 break;
		 	 case 0x719:
		 		 UDS_DIAG_rcv(RxFrame);
		 		 UDSFlag ++;
		 		 break;
		 	 case 0x700:
		 		 DCDC700_rcv(RxFrame, &rx_dcdc700); //Receive frame
		 		 DCDC700_memHandler(rx_dcdc700, DCDC_700); //handle memory
		 		 break;
		 	 case 0x703:
		 		 DCDC703_rcv(RxFrame, &rx_dcdc703); //Receive frame
		 		 break;
		 	 default:
		 		 sprintf(msg, "Unknown ID in FIFO 1\r\n");
		 		 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
		 		 break;
		 }
	 }
}

imultaneously. Then i used only one to receive the frames and it works.

11 replies

mƎALLEm
ST Technical Moderator
May 16, 2024

Hello,

Try first with "passing all messages" filter to be sure it's not a filter config issue:

 

canfilterconfig.FilterIdHigh = 0,
canfilterconfig.FilterIdLow = 0;
canfilterconfig.FilterMaskIdHigh = 0;
canfilterconfig.FilterMaskIdLow = 0;

 

PS: next time please use <\> button to insert your code. Thank you for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Erwan03Author
Associate III
May 16, 2024

Hello thank you for your quick answer.

 

I did what you said put 0 to cancel the filter. but nothing changed, here is a code of the following files: main.c; CanfilterConfig.c

 

main

void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
	HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &RxHeader, RxFrame);
	 {
		 switch(RxHeader.StdId)
		 {
			 case 0x586:
				 BatteryChargeCurrent_rcv(RxFrame, &rx_BCC); //Receive frame
				 BatteryChargeCurrent_memHandler(rx_BCC, &h_BCC); //handle memory
				 BCCFlag++;
				 break;
			 case 0x591:
				 BatteryCurrentLimit_rcv(RxFrame, &rx_BCL); //Receive frame
				 BatteryCurrentLimit_memHandler(rx_BCL, h_BCL); //handle memory
				 BCLFlag++;
				 break;
			 case 0x587:
				 BatteryStatusCharge_rcv(RxFrame, &rx_BSC); //Receive frame
				 BatteryStatusCharge_memHandler(rx_BSC, h_BSC); //handle memory
				 BSCFlag++;
				 break;
			 case 0x580:
				 BatteryStatusGeneral_rcv(RxFrame, &rx_BSG); //Receive frame
				 BatteryStatusGeneral_memHandler(rx_BSG, h_BSG); //handle memory
				 BSGFlag++;
				 break;
			 case 0x59f:
				 BatteryVehicleHandling_rcv(RxFrame, &rx_BVH); //Receive frame
				 BatteryVehicleHandling_memHandler(rx_BVH, h_BVH); //handle memory
				 BVHFlag++;
				 break;
			 default:
				 sprintf(msg, "Unknown ID in FIFO 0\r\n");
				 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
				 break;
		 }
	 }
}

int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */
 DID_Init();
 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_USART2_UART_Init();
 MX_CAN1_Init();
 MX_ADC1_Init();
 MX_TIM6_Init();
 /* USER CODE BEGIN 2 */
 CAN_Filter_FIFO0(&hcan1); // Filter config for FIFO0
 CAN_Filter_FIFO1(&hcan1); // Filter config for FIFO1
 HAL_CAN_Start(&hcan1);

 HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING); // Enable Interrupt at FIFO0 reception
 HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO1_MSG_PENDING); // Enable Interrupt at FIFO1 reception

 HAL_TIM_Base_Start_IT(&htim6); // Start timer for scheduled frame sending
 //HAL_ADC_Start_IT(&hadc1); // Start adc

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 uint8_t countpres;
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
//	 if (uADCConversionCpltFlag) {
//	 		uiADCRawValueBuffer = HAL_ADC_GetValue(&hadc1);
//	 		sprintf(msg, "Throttle: %hu \r\n", uiADCRawValueBuffer);
//	 		HAL_UART_Transmit(&huart2, (uint8_t *)msg, strlen(msg), HAL_MAX_DELAY);
//	 	}

	 /*Single channel polling*/
//		HAL_ADC_Start(&hadc1);
//		HAL_ADC_PollForConversion(&hadc1, HAL_MAX_DELAY);
//		uiADCRawValueBuffer = HAL_ADC_GetValue(&hadc1);
//		sprintf(msg, "Throttle: %hu \r\n", uiADCRawValueBuffer);
//		HAL_UART_Transmit(&huart2, (uint8_t *)msg, strlen(msg), HAL_MAX_DELAY);

	 /****************** USABLE CODE ******************/

	 /*SEND UDS RESPONSE*/

	 if(UDSFlag!=0)
	 {
		 UDSFlag = 0;
		 UDS_Response_mgt(RxFrame, VCU_Response, &TxHeader, TxFrame);
		 CAN_Send_Periodic();
	 }

	 if(BCCFlag!=0)
	 {
		 BCCFlag = 0;
		 Discharge_Battery();
		 Discharge_DCDC();
		 sprintf(msg, "BatteryChargeCurrent frame received\r\n");
		 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
	 }

	 if(BCLFlag!=0)
	 {
		 BCLFlag = 0;
		 Discharge_Battery();
		 Discharge_DCDC();
		 sprintf(msg, "BatteryCurrentLimit frame received\r\n");
		 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
	 }

	 if(BSCFlag!=0)
	 {
		 BSCFlag = 0;
		 Discharge_Battery();
		 Discharge_DCDC();
		 sprintf(msg, "BatteryStatusCharge frame received\r\n");
		 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
	 }

	 if(BSGFlag!=0)
	 {
		 BSGFlag = 0;
		 Discharge_Battery();
		 Discharge_DCDC();
		 sprintf(msg, "BatteryStatusGeneral frame received\r\n");
		 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
	 }
 }
}

 

CanFilterConfig

#include "CanFilterConfig.h"


void CAN_Filter_FIFO0(CAN_HandleTypeDef* hcan)
{
	 CAN_FilterTypeDef canfilterconfig;

	 canfilterconfig.FilterActivation = CAN_FILTER_ENABLE;
	 canfilterconfig.FilterBank = 10;
	 canfilterconfig.FilterFIFOAssignment = CAN_FILTER_FIFO0;
	 canfilterconfig.FilterIdHigh = 0x580 << 5; // According to the DBC
	 canfilterconfig.FilterIdLow = 0x0000;
	 canfilterconfig.FilterMaskIdHigh = 0xfe0 << 5;// Calculation of the mask according to the DBC
	 canfilterconfig.FilterMaskIdLow = 0x0000;
	 canfilterconfig.FilterMode = CAN_FILTERMODE_IDMASK;
	 canfilterconfig.FilterScale = CAN_FILTERSCALE_32BIT;
	 canfilterconfig.SlaveStartFilterBank = 13;

	 HAL_CAN_ConfigFilter(hcan, &canfilterconfig);
}

 

Thank you again for your time

mƎALLEm
ST Technical Moderator
May 16, 2024

Hello,

Better to attach your main.c and your ioc files.

+ keep the filters to 0 for the moment.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Erwan03AuthorBest answer
Associate III
May 21, 2024

Alright, found the problem, I was using both fifo0 and fifo1 for receiving whereas i had to use only one for all the frames. Don't know how to use both of them s

void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
	HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &RxHeader, RxFrame);
	 {
		 switch(RxHeader.StdId)
		 {
		 	 case 0x586:
				 BatteryChargeCurrent_rcv(RxFrame, &rx_BCC); //Receive frame
				 BatteryChargeCurrent_memHandler(rx_BCC, &h_BCC); //handle memory
				 BCCFlag++;
				 break;
		 	case 0x591:
				 BatteryCurrentLimit_rcv(RxFrame, &rx_BCL); //Receive frame
				 BatteryCurrentLimit_memHandler(rx_BCL, h_BCL); //handle memory
				 BCLFlag++;
				 break;
			 case 0x587:
				 BatteryStatusCharge_rcv(RxFrame, &rx_BSC); //Receive frame
				 BatteryStatusCharge_memHandler(rx_BSC, h_BSC); //handle memory
				 BSCFlag++;
				 break;
			 case 0x580:
				 BatteryStatusGeneral_rcv(RxFrame, &rx_BSG); //Receive frame
				 BatteryStatusGeneral_memHandler(rx_BSG, h_BSG); //handle memory
				 BSGFlag++;
				 break;
			 case 0x59f:
				 BatteryVehicleHandling_rcv(RxFrame, &rx_BVH); //Receive frame
				 BatteryVehicleHandling_memHandler(rx_BVH, h_BVH); //handle memory
				 BVHFlag++;
				 break;
		 	 case 0x24:
		 		 EPIC_PMZ_A_rcv(RxFrame, &rx_pmzA); //Receive frame
		 		 EPIC_PMZ_A_memHandler(rx_pmzA, h_PMZ_A); //handle memory
		 		 break;
		 	 case 0x50:
		 		 EPIC_PMZ_C_rcv(RxFrame, &rx_pmzC); //Receive frame
		 		 EPIC_PMZ_C_memHandler(rx_pmzC, h_PMZ_C); //handle memory
		 		 break;
		 	 case 0x5A:
		 		 EPIC_PMZ_E_rcv(RxFrame, &rx_pmzE); //Receive frame
		 		 EPIC_PMZ_E_memHandler(rx_pmzE, h_PMZ_E); //handle memory
		 		 break;
		 	 case 0x5E:
		 		 EPIC_PMZ_G_rcv(RxFrame, &rx_pmzG); //Receive frame
		 		 EPIC_PMZ_G_memHandler(rx_pmzG, h_PMZ_G); //handle memory
		 		 break;
		 	 case 0x60:
		 		 EPIC_PMZ_H_rcv(RxFrame, &rx_pmzH); //Receive frame
		 		 EPIC_PMZ_H_memHandler(rx_pmzH, h_PMZ_H); //handle memory
		 		 break;
		 	 case 0x4e2:
		 		 EPIC_PMZ_I_rcv(RxFrame, &rx_pmzI); //Receive frame
		 		 EPIC_PMZ_I_memHandler(rx_pmzI, &h_PMZ_I); //handle memory
		 		 break;
		 	 case 0x621:
		 		 HMI_DATA1_rcv(RxFrame, &rx_cluster); //Receive frame
		 		 HMI_DATA1_memHandler(rx_cluster, h_HMI); //handle memory
		 		 break;
		 	 case 0x719:
		 		 UDS_DIAG_rcv(RxFrame);
		 		 UDSFlag ++;
		 		 break;
		 	 case 0x700:
		 		 DCDC700_rcv(RxFrame, &rx_dcdc700); //Receive frame
		 		 DCDC700_memHandler(rx_dcdc700, DCDC_700); //handle memory
		 		 break;
		 	 case 0x703:
		 		 DCDC703_rcv(RxFrame, &rx_dcdc703); //Receive frame
		 		 break;
		 	 default:
		 		 sprintf(msg, "Unknown ID in FIFO 1\r\n");
		 		 HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
		 		 break;
		 }
	 }
}

imultaneously. Then i used only one to receive the frames and it works.

mƎALLEm
ST Technical Moderator
May 21, 2024

Hello,

You can use them both simultaneously. According to the code source you shared at the beginning I don't see an issue.

For each FIFO you can set a filter config, so you will receive the matching message on that FIFO.

Maybe you didn't explain or provide more details of what you intended to do...

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.