Skip to main content
Associate II
Jul 19, 2017 9:10 PM UTC
Solved

Issue re-enabling LPUART1 receiver?

Posted on July 19, 2017 at 23:10

I have a circuit that requires the receiver to be disabled when transmitting and the transmitter disabled while receiving. I seem to be having trouble re-enabling the receiver after transmitting a packet of data. 

I do not get any UART interrupts on the next receive event. I have trapped it with the debugger and the UART register shows the receiver is enabled, the receive interrupt is enabled, and the uart is enabled. The only thing I do not see is the REACK flag set. If I try to sit in a loop until REACK is set, I end up in a infinite loop.

I can receive a packet, switch to transmit and send a packet, but I am unable to successfully switch back into a valid receive mode. This is all part of a exchange of data without any gaps between packets and I am not going to sleep between packets. 

Processor: STM32L011

Module: LPUART1

void enable_uart_transmitter(void)

{

     LPUART1->CR1 |= ( USART_CR1_TXEIE | USART_CR1_TE );

}

void disable_uart_transmitter(void)

{

     LPUART1->CR1 &= ~(USART_CR1_TXEIE | USART_CR1_TCIE | USART_CR1_TE);

}

void enable_uart_receiver(void)

{

      LPUART1->CR1 |= ( USART_CR1_RXNEIE | USART_CR1_RE );

}

void disable_uart_receiver(void)

{

     LPUART1->CR1 &= ~( USART_CR1_RXNEIE | USART_CR1_RE );

}

    This topic has been closed for replies.
    Nick McKendreeBest answer
    Associate II
    Jul 20, 2017 2:04 PM UTC
    Posted on July 20, 2017 at 16:04

    Problem solved. 

    Issue relating the UART RX set to GPIO during TX but never switched back to alternate mode during receive period. 

    1 reply

    Nick McKendreeAuthorBest answer
    Associate II
    Jul 20, 2017 2:04 PM UTC
    Posted on July 20, 2017 at 16:04

    Problem solved. 

    Issue relating the UART RX set to GPIO during TX but never switched back to alternate mode during receive period.