Skip to main content
Associate III
Oct 2, 2024 4:39 AM UTC
Solved

Issue After Bootloader on STM32F072RBT6: Stack Pointer Not Jumping to Application Address

Dear STM32 Community,

I am currently working on a project using the STM32F072RBT6 microcontroller, where I have implemented a custom bootloader to load an application program into flash memory. However, after the bootloader successfully writes the application binary, the stack pointer does not correctly jump to the application’s address, and the application fails to execute. 

MCU Model: STM32F072RBT6 Bootloader

Functionality: The bootloader receives the application binary and writes it to flash memory at the designated application address.

Application Flash Address: 0x08004000

Problem: After the bootloader completes, I attempt to jump to the application by setting the stack pointer and program counter accordingly, but the application does not start. It appears that the stack pointer is not correctly set to the application's address.

Jump Code in Bootloader:

 

static void goto_application(void){

void (* app_reset_handler)(void) = (void *)(*(volatile uint32_t *) (0x08004000 + 4));

__disable_irq();

__set_MSP((*(volatile uint32_t *)0x08004000));

__enable_irq();

app_reset_handler();

}

This topic has been closed for replies.
shyamparmarBest answer
Associate III
Oct 9, 2024 11:30 AM UTC

Dear STM32 Community,

I hope this message finds you well. I wanted to take a moment to express my sincere thanks to everyone who contributed their time and expertise to help me with my issue. I’m happy to report that I’ve successfully solved the problem!

The issue was related to the HAL_Delay function in my application code. I was using HAL_Delay incorrectly, which caused my application code to get stuck. After going through the suggestions and feedback from the community, I was able to identify and resolve the root cause.

Thank you once again for your invaluable support and insights. I appreciate being part of such a knowledgeable and helpful community! 

23 replies

Tesla DeLorean
Guru
Oct 2, 2024 9:51 AM UTC

So it is set to WHAT exactly?

The use of auto/local variables whilst changing the SP is also seriously ill advised.

Look at the generated code.

Do this stuff in assembler, or have the apps Reset_Handler set SP when you get there.

The F0 is also a CM0 so no SCB->VTOR, vectors need to get copied to RAM and remapped.

.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate III
Oct 4, 2024 6:10 AM UTC

@Tesla DeLorean  "Thanks for the input! I tried remapping the vectors for the STM32F032RBT6 and handling the reset in the application, but it still gets stuck somewhere in the code. Any ideas on what might be causing this?"

TDK
Oct 2, 2024 12:23 PM UTC

Are interrupts active in the bootloader? You'll need to disable them first.

When it "doesn't start" where is execution at?

There is nothing wrong with the code you've presented. The problem lies elsewhere. General code for jumping to the bootloader can be found here. You can adapt it for jumping to the application.

How to jump to system bootloader from application ... - STMicroelectronics Community

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate III
Oct 4, 2024 6:16 AM UTC

@TDK "Yes, I’m using the UART receive interrupt in the bootloader to receive the application binary file. After that, I want to jump from the bootloader to the application code. Do I need to disable interrupts before jumping? Any advice on handling the transition would be helpful!" 

TDK
Oct 4, 2024 1:14 PM UTC

Look at the code I linked. You must disable the UART interrupt before jumping so it isn't called when the bootloader is running. This is what clearing the ICER/ICPR registers does. You should not globally disable interrupt.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Pavel A.
Oct 2, 2024 1:06 PM UTC

Besides of possible reasons mentioned by TDK and Tesla... consider effects of compiler optimization.

Variable app_reset_handler is local and it may be allocated on the stack.

Then you move the stack pointer. This is what __set_MSP does. It changes the stack pointer.

Guess what happens to the app_reset_handler variable?

 

Associate II
Oct 3, 2024 1:49 AM UTC

Exactly. The bootloader code that STM32CubeMX generates suffers from this same issue. When optimizations are enabled (with AC6 anyway) it works fine. But crashes when using -O0. 

Associate III
Oct 4, 2024 5:55 AM UTC

@mbrossett  "Thanks for the suggestion! I already tried changing the optimization level, but unfortunately, the same problem occurs even with different settings, including -O0. It seems like the issue persists regardless of the optimization level. Any other ideas on what could be causing this?"