Skip to main content
Imla
Associate
January 31, 2022
Question

Is this a correct code modification?

  • January 31, 2022
  • 5 replies
  • 1081 views

// stm32f1xx_hal_rtc.c line 827

sTime->Seconds = (uint8_t)((counter_time % 3600U) % 60U);

// to this

sTime->Seconds = (uint8_t)(counter_time % 60U);

This topic has been closed for replies.

5 replies

Peter BENSCH
ST Technical Moderator
January 31, 2022

Welcome, @Imla​, to the community!

This particular case with 3600 and 60 can indeed be shortened to 60, but it cannot be generalised. For example, if you want to shorten ((counter_time % 20U) % 5U) to (counter_time % 4U), it will only fit in 80% of the cases, which is due to the mathematical peculiarity of modulo.

Good luck!

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
waclawek.jan
Super User
January 31, 2022

> ((counter_time % 20U) % 5U) to (counter_time % 4U), it will only fit in 80% of the cases

Only 20% of the cases... ((counter_time % 20U) % 5U) is equivalent to (counter_time % 5U).

JW

Peter BENSCH
ST Technical Moderator
January 31, 2022

Oops, yes, I did a mistake and Jan is right:

((X mod Y) mod Z) can be shortened to (X mod Z)

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Imla
ImlaAuthor
Associate
January 31, 2022

I know the math... But I'm still wondering about the reasons behind that code?! given that the compiler did not optimize the code with a single expression (counter_time % 3600U) % 60U) ...I didn't checked the version where the expression (counter_time % 3600U) used twice at the same code...anyway stm32 has a plenty of SRAM and I must forget Attiny at least for now.

Danish1
Lead III
February 1, 2022

I wonder if it is an attempt to force the compiler to do the conversion-to-8-bits at a time when it won't garble the result.

I don't know the width of counter-time, but it seems reasonable to assume it is wider than 8 bits.

If an optimiser were to look at code that said (uint8_t)(a <op> b) where b fitted into uint8_t, would it try to convert the code to ((uint8_t)a) <op> b?

Probably not on stm32, but one can imagine that being considered for an 8-bit microcontroller (I'm more familiar with PIC16 than AtTiny), where even 16-bit arithmetic is expensive.

There's a lot of "history" in code. If it's known to work, and is not too inefficient, then is it worth the risk of rewriting it and possibly introducing new bugs?