Question
Is this a bug that STM32H743 HAL_ADC_Stop_DMA clears ADC_CFGR_DMNGT?
Posted on August 21, 2017 at 11:48
Hello,
In the line 1760 of 'stm32h7xx_hal_adc.c' in pack 'STM32H7xx_DFP 1.0.1':
'''
/* Disable ADC DMA (ADC DMA configuration ADC_CFGR_DMNGT is kept) */
MODIFY_REG(hadc->Instance->CFGR, ADC_CFGR_DMNGT_0 |ADC_CFGR_DMNGT_1, 0);
'''
The comment says 'keep the DMNGT' while the code actually clears it. Besides
it doesn't make much sense to me that calling a 'HAL_ADC_Stop_DMA' could change the initial configuration of ADC.
Is this a bug? Or 'HAL_ADC_Stop_DMA' is not something I should call under normal condition?