Question
Is there some sort of foiling problem with PA6 on the NUCLEO-L496ZG board?
Is there some sort of foiling problem with PA6 on the NUCLEO-L496ZG board? I am trying to setup PA6 to be the OPAMP2 positive input. There always seems to be 3 volts stuck on this pin with nothing connected. PA0 works just fine when configured for OPAMP1 plus input. I even bought another board and same thing. Applying signals to both pins yields correct adc readings but OPAMP1 out is just always biased. I have tried everything! I'm using latest CubeMX