Is there any way to set a specific GPIO high when entered a bootloader
I am programming the uC via UART that is connected via a Transceiver. The transceiver has an DE (Driver Enable) pin which is active high. Unfortunately, it has a pull down instead of pull-up in a design, therefor the uC can hear but can't talk back. This pin (DE) is also connected to one of the uC GPIOs. If only I could set this pin high by sending something to the uC when its in the boot-loader mode.., can I?
Other thought would be to force the STM32Cube to connect.. as off it has received the 0x7F from the uart.
Please help.