Is there any way to expand the CAN filters on STM32 MCUs using external Hardware?
Hello,
I have been looking to read almost 200 different Extended CAN Ids on any of the CAN equipped STM32 MCUs. Speed in 1Mbps on CAN.
Currently, I am working with ID list mode using all 28 filters and switching between CAN Ids as required. But I am facing slight data loss which I am trying to avoid. Is there any method to expand the 28 filters to 200 by using some external filtering ICs? To pump up speeds, I am already using PLL on the MCU and a decent CAN Transceiver. I also wrote code using STD Periph libraries to optimize as much as I could. I cannot simply turn off all filtering as those 200 IDs are not the only IDs I am receiving on the CAN port.