Skip to main content
KSkor.1
Associate III
Feb 18, 2021 2:14 PM UTC
Solved

Is there any app, similar to "st-link utility" that i could use with a android tablet?

Hi,

i develop 100% of my code in my workshop or office, but sometimes i wish i could do some very light modification to a parameter or baud or something in the field and i dont really fancy carrying my expensive workstation laptop around.

So i wonder if there is an app for android (or ios) similar to stlink utlity, so i could connect st-link debuger via otg usb to tablet and flash new code(modifing can be done easly in any notepad type app) in the field?

    This topic has been closed for replies.
    Andrew Neil
    Andrew NeilBest answer
    Super User
    Feb 19, 2021 1:53 PM UTC

    "what exactly deaf and drop programming is? Google does not find anything useful"

    :face_with_tears_of_joy:

    Pretty sure that should be, "drag and drop" ?!

    ie, where the ST-Link appears as a USB Mass-Storage Device, so you can just drag your .bin file from wherever you keep it, and drop it onto the ST-Link's MSD.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

    9 replies

    Uwe Bonnes
    Chief
    Feb 18, 2021 2:42 PM UTC

    Any STLINK > V1 offers a mass storage device for deaf-and drop programming.Is'nt that what you need?

    KSkor.1
    KSkor.1Author
    Associate III
    Feb 19, 2021 8:57 AM UTC

    can you post link to a white paper or some explanation of what exactly deaf and drop programming is? Google does not find anything useful.

    Andrew Neil
    Andrew NeilBest answer
    Super User
    Feb 19, 2021 1:53 PM UTC

    "what exactly deaf and drop programming is? Google does not find anything useful"

    :face_with_tears_of_joy:

    Pretty sure that should be, "drag and drop" ?!

    ie, where the ST-Link appears as a USB Mass-Storage Device, so you can just drag your .bin file from wherever you keep it, and drop it onto the ST-Link's MSD.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Javier1
    Principal
    Feb 18, 2021 4:58 PM UTC

    you could try remote desktops, aydesk works well for me

    hit me up in https://www.linkedin.com/in/javiermuñoz/
    KSkor.1
    KSkor.1Author
    Associate III
    Feb 19, 2021 8:56 AM UTC

    thk, will try with aydesk. Tried to make it work with google remote desktop, but didnt have any luck with sharing tablet USB port with pc running the St-link.

    Javier1
    Principal
    Feb 19, 2021 10:03 AM UTC

    *anydesk (typo)

    hit me up in https://www.linkedin.com/in/javiermuñoz/
    Andrew Neil
    Super User
    Feb 19, 2021 1:56 PM UTC

    "some very light modification to a parameter or baud or something in the field"

    Surely, it would be far better to give your app a configuration interface for such changes - not the kind of thing you want to be rebuilding the code for?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    KSkor.1
    KSkor.1Author
    Associate III
    Feb 22, 2021 12:47 PM UTC

    depends on the project. Most of mine are compiled in few seconds, maybe half a minute tops, so really, rebuilding code is not a problem. And tried this weekend using CubeIDE and anydesk remote, with drag and drop programing via stlink. it all work together as a charm.

    But yea, in case of big project with budget for development of interface to set parameters via usb connection and a simple terminal program on tablet side, this is viable solution.