Skip to main content
Stefan W
Associate II
Apr 4, 2017 12:50 PM UTC
Solved

Is there an version of OpenOCD with support for the STM32F413

Posted on April 04, 2017 at 14:50

Hi,

I tried to connect to the STM32F413 with OpenOCD, but I get the following error:

Info : device id = 0x10006463

Warn : Cannot identify target as a STM32 family.

Error: auto_probe failed

I searched the source code of OpenOCD 0.10.0 and it seems as if the F413 is not yet supported. Does anyone has a patched version of OpenOCD with support for the STM32F413?

Best regards,

Stefan

#openocd #stm32f413
This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Apr 4, 2017 2:32 PM UTC
Posted on April 04, 2017 at 16:32

You know they have a mailing list?

https://sourceforge.net/p/openocd/mailman/message/33251369/

 

The patch would be pretty trivial, at least to get basic functionality, ie recognize the 0x463 Device ID and set memory sizes. Try it, it shouldn't be that hard.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Apr 4, 2017 2:32 PM UTC
Posted on April 04, 2017 at 16:32

You know they have a mailing list?

https://sourceforge.net/p/openocd/mailman/message/33251369/

 

The patch would be pretty trivial, at least to get basic functionality, ie recognize the 0x463 Device ID and set memory sizes. Try it, it shouldn't be that hard.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Stefan W
Stefan WAuthor
Associate II
Apr 5, 2017 9:06 AM UTC
Posted on April 05, 2017 at 11:06

Hi,

that's right. Adding the device id to OpenOCD was not very hard. It was much harder to compile OpenOCD for Windows, but I finally could compile a basic version with at least support for the st-link.

Another issue was to update the ST Link Adapter's firmware. With the old firmware there was a cryptic error message about address wrapping.

Now I can start porting my application to the STM32F413.