Question
Is there a listing of the program that come loaded on the STM32 Nucleo L031 board?
Posted on August 28, 2017 at 18:22
Hi Folks,
I've just started working with the STM32 NucleoL031 board and I think it would help me understand the system if I can find a listing of the program that is pre-loaded on the chip. It blinks the green LED at one rate and if you put the jumper on that connects GND with D2 it will blink at a slower rate.
I've searched through the ST site but can't seem to find it.
Thanks in advance,
Richard
#nucleo-l031 #nucleo #l031