Skip to main content
luke514
Associate III
January 8, 2023
Question

Is there a built-in microphone in the STM32F407?

  • January 8, 2023
  • 3 replies
  • 2088 views

This is the first time I have used an STM32F4 board.

In the Discovery kit with STM32F407VG MCU I see "one digital microphone", but I don't understand if it's already integrated in the board or I have to buy it separately.

If it is included, can you tell me in which manual I can find its specifications?

User manual? Reference manual? I'm searching but with no results.

Thanks!

This topic has been closed for replies.

3 replies

KnarfB
Super User
January 8, 2023

It is a MP45DT02 on the board (U9), not in the chip. See UM1472 user manual and schematics mb997-f407vgt6-b02_schematic.pdf (revision code may vary).

hth

KnarfB

luke514
luke514Author
Associate III
January 8, 2023

Thanks!

I have a couple of questions:

1) In the UM1472 (rev.7) user manual there's written that "Revision E-01" replaces the MP45DT02-M microphone (U9) with the IMP34DT05TR.

It is not clear to me which of these two microphones I have on board on my board.

2) I checked all the official documentation of the STM32F407-DISC1 but only found informations about the microphone in the application note AN3997 'Audio-playback-and-recording' which provides an example and the related library explained in AN3998 'PDM-audio-software-decoding'.

I will study these files but ask if you know of any other files/tutorials that explain the mic implementation step by step. 

KnarfB
Super User
January 8, 2023

1) the revision letter is in the top right corner of the board M997..

2) no, but I haven't done a deep search.

hth

KnarfB