Skip to main content
JSils
Associate
August 20, 2018
Question

Is the STULPI01 compatible for HS USB functionality with the STM32H743?

  • August 20, 2018
  • 2 replies
  • 896 views

Hi,

I have read a few forum posts on here with regards to STM32's working with specific USB PHYs. There is a lot of confirmation that the MicroChip USB3320 works with specific STM32's. In fact the dev kit for the STM32H743 (which is the Micro I am using) has a USB3320 on it.

My question is:

Why aren't the ST ULPI USB PHYS, STUPLI01, on the ST dev kits?

Is the STUPLI01 compatible with the STM32H743, for HS USB data transfers?

Thanks in Advance,

Jack

This topic has been closed for replies.

2 replies

LoriB
Associate
October 1, 2018

I think your question is a rightful one and I wonder the same thing.

I can tell tou that I have a design with an STM32F7 and an STULPI01B that works fine.

Actually I have some stall issues during long streams, but I think they are closely related to my hardware configuration.

JSils
JSilsAuthor
Associate
April 8, 2019

​​Hi LoriB,

Thanks for your answer.

I finally have some PCBs with the ST32 and the PHY on but we are having trouble deciphering the software commands to put the PHY into HS Peripheral mode. 

From what I can tell I need to write data 0x40 to the Function Control register and data 0x00 to the OTG register.

I am confused by the addresses of these registers though:

The Function Control register for example (Pg 32 of the datasheet) states: 

Read (04H-06H),

Write (04),

Set (05),

Clear (06)

How can read cover all the addresses - how do we differentiate between a read and a write for example?

I have seen that, you must put a TXCMD on the ULPI data pins (0x10XXXXXX for read and 0x11XXXXXX for write)

But why does Figure.10 High-speed mode entry show 0x84, 0x50 being written to the ULPI?

I have to admit I find the datasheet for this device incredibly difficult to follow!

Could you please help me to understand this better?

Thanks,

Jack