Skip to main content
M. Jeong
Associate III
March 12, 2017
Question

Is the DCMI capable of acquiring 12-bit raw bayer image data?

  • March 12, 2017
  • 3 replies
  • 791 views
Posted on March 12, 2017 at 14:08

The data sheet of the STM32F429 shows that its camera interface can take 14-bit parallel data and the maximum data rate is 54MB/s. Also it says the interface supports 8-bit progressive video monochrome or raw bayer format, without mentioning higher bitdepth. I wonder if it does imply that you can't capture 10-bit or 12-bit raw bayer image data with the DCMI.

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    March 12, 2017
    Posted on March 12, 2017 at 14:17

    I believe it is agnostic to the form of the data

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    M. Jeong
    M. JeongAuthor
    Associate III
    March 12, 2017
    Posted on March 12, 2017 at 14:44

    The table 18 on the following document shows 14-bit raw bayer format is supported. But I'm not sure why the data sheet doesn't mention 10, 12, 14-bit.  

    http://www.st.com/content/ccc/resource/technical/document/application_note/26/22/fe/1d/f1/ca/4c/08/DM00161778.pdf/files/DM00161778.pdf/jcr:content/translations/en.DM00161778.pdf

     

    Also it's strange that the ST wrote '8/10, 12, 14 bits progressive video (monochrome or raw bayer) '. What does '8/10' mean...?  Why are there two same items in the 'supported data format' box? 

    Tesla DeLorean
    Guru
    March 12, 2017
    Posted on March 12, 2017 at 15:32

    8 or 10-bit modes

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..