Skip to main content
bl_it
Associate III
April 12, 2013
Question

Is Systick the way to generate a delay function

  • April 12, 2013
  • 3 replies
  • 1046 views
Posted on April 12, 2013 at 08:49

Hi Folks (and Clive)

I have generated timing delays using systick and I want some comments on whether it was the right way to go:-

GPIO_InitTypeDef GPIO_InitStructure;

static __IO uint32_t TimingDelay;

void Delay(__IO uint32_t nTime)

    {

    TimingDelay = nTime;

    while (TimingDelay != 0)

;

    }

void TimingDelay_Decrement(void)

    {

    if (TimingDelay != 0x00)

{

TimingDelay--;

}

    }

extern ''C'' void SysTick_Handler(void)

    {

    TimingDelay_Decrement();

    }

I believe that systick is a low priority - so can this code get stuck if there is a pending higher priority interrupt??

CS

    This topic has been closed for replies.

    3 replies

    zzdz2
    Associate
    April 12, 2013
    Posted on April 12, 2013 at 11:29

    I make short delays without interrupts:

    #define TICKSGN ((SysTick_VAL_CURRENT_Msk+1)>>1)
    #define WAITMAX (SysTick_VAL_CURRENT_Msk >> 1)
    static inline void waittick(uint32_t step)
    {
    static uint32_t tick0;
    if (!step)
    {
    tick0 = SysTick->VAL;
    return;
    }
    tick0 -= step;
    while ((tick0 - SysTick->VAL) & TICKSGN)
    {
    __NOP();
    __NOP();
    }
    }
    static inline void sleep(uint32_t delay)
    {
    waittick(0);
    delay++;
    while (delay > WAITMAX)
    {
    waittick(WAITMAX);
    delay -= WAITMAX;
    }
    waittick(delay);
    }

    Tesla DeLorean
    Guru
    April 12, 2013
    Posted on April 12, 2013 at 13:30

    You can change the priority of the SysTick interrupt. Generally speaking you shouldn't be spending enough time in another interrupt for this to be a problem, or using multi millisecond delays in other interrupt routines.

    My preference would be for SysTick to increment a millisecond tick variable continuously, and have the delay routine observe that. For finer precision, delays could also use DWT_CYCCNT
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    bl_it
    bl_itAuthor
    Associate III
    April 16, 2013
    Posted on April 16, 2013 at 10:20

    Hi folks 

    Thanks for your comments - its good to know I'm not fundamentally going in the wrong direction!! I will have a look at the suggestions for other types of delays as I'm sure they will be useful.

    CS