Skip to main content
kk6gm
Associate II
September 29, 2011
Question

Is PB5 really not 5V tolerant?

  • September 29, 2011
  • 4 replies
  • 1125 views
Posted on September 29, 2011 at 18:35

The data sheet I have says it isn't, and yet it's not an ADC input as all the other non 5V tolerant pins seem to be.  Of course I'll believe the datasheet if there's no positive information that it's wrong, but it seems suspicious enough (and datasheets have been known to be wrong!) that I thought I'd ask if anybody has better info.

    This topic has been closed for replies.

    4 replies

    donald2
    Associate
    September 29, 2011
    Posted on September 29, 2011 at 21:04

    Grrrr, the board software discarded my first response.

    Short answer (because I'm not willing to recreate the previous long message): PB5 is buggy.  It's bitten me twice. It's likely that this pin was intended to be 5V tolerant, but the same bugs that broke MOSI and TIM3 output also broke the protection structure.

    kk6gm
    kk6gmAuthor
    Associate II
    September 29, 2011
    Posted on September 29, 2011 at 21:41

    OK, thanks for clearing up that mystery.

    donald2
    Associate
    September 29, 2011
    Posted on September 29, 2011 at 23:19

    Also, to be safe, assume PB5 still has the restriction of 5V-tolerant pins and cannot accept injected current.  (Regular pins allow 5 mA, which means you can sense higher voltage with just a high value resistor. 5V pins must be protected with both a resistor and a Schottky diode to Vdd.)

    kk6gm
    kk6gmAuthor
    Associate II
    September 29, 2011
    Posted on September 29, 2011 at 23:38

    Ah, I didn't know about that ability.  Thanks for pointing it out.