Skip to main content
HAbay.1
Associate III
Aug 6, 2021 10:35 PM UTC
Solved

Is it possible to use the RTC alarm signal on the tamper pin in order to turn on a transistor or maybe hold that value in a D flip flop?

I've been doing a lot of research concerning Low power modes for the stm32 bluepill and I was wondering if i could power my board through VDD and execute a code through it and then right after going into sleep mode I would use a switch to only power the board through Vbat to save power , but the problem here is that the alarm wake up for the rtc won't be able to wake the board up from Vbat so my question is: is there a way to say store that rising edge from the rtc tamper pin and use it to switch back from Vbat to vdd?

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Aug 9, 2021 11:17 AM UTC

Blue pill is now very often populated with clones that do not behave identically to the origina STM32F103C8T6l. So first you should check whether there is a clone or the original F103 on the Blue pill.

The F103 can be operated in stand-by mode and would then only draw approx. 2µA at VDD and 1.4µA µA at VBAT.

Does your external circuit need less current than the above mentioned 2µA to switch off VDD and to detect a switch-on process?

If you really want to save power, you should therefore look at more modern MCUs that are significantly more power efficient, e.g. the STM32L0, STM32L4 or STM32L4+.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Aug 9, 2021 11:17 AM UTC

Blue pill is now very often populated with clones that do not behave identically to the origina STM32F103C8T6l. So first you should check whether there is a clone or the original F103 on the Blue pill.

The F103 can be operated in stand-by mode and would then only draw approx. 2µA at VDD and 1.4µA µA at VBAT.

Does your external circuit need less current than the above mentioned 2µA to switch off VDD and to detect a switch-on process?

If you really want to save power, you should therefore look at more modern MCUs that are significantly more power efficient, e.g. the STM32L0, STM32L4 or STM32L4+.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.