Skip to main content
RemoF
Associate
Jun 17, 2020 4:26 PM UTC
Question

Is it possible to use Serial SRAM (QSPI) with the STM32H743?

Hi all

I have a custom Board with STM32H743 and i would like to add external SRAM and NOR Flash at the QSPI Interface. For example the SRAM at the Bank1 and the Flash at Bank2.

Is this possible?

I' would like to use for SRAM:

https://www.mouser.ch/ProductDetail/ISSI/IS62WVS5128GBLL-45NLI?qs=byeeYqUIh0M7EH7gI3DsmQ%3D%3D

and for Flash:

https://www.mouser.ch/ProductDetail/ISSI/IS25LP032D-JNLE?qs=DXv0QSHKF4z8ea2r8jlMmA%3D%3D

Thanks

#SRAM​  #[STM32 MCUs]​ #QSPI​ #STM32H7​ 

This topic has been closed for replies.

3 replies

berendi
Principal
Jun 18, 2020 9:19 AM UTC

Yes, but ...

  • Only one of them can be accessed at the same time (but the RAM can be accessed while the flash is busy erasing/writing sectors)
  • Memory mapped mode is read-only.
  • It can be slow.
RemoF
RemoFAuthor
Associate
Jun 23, 2020 9:17 AM UTC

And if i use only SRAM

Is it possible to get the Access to QSPI SRAM like this?

Scatter File:

...
 RW_RAM2 0x90000000 0x00080000 {
 *.o (ExRAM) 
 }
...

I would like to access the section ExRAM like this:

...
uint16_t Array[1024] __attribute__((section("ExRAM")));
...

Thanks

berendi
Principal
Jun 23, 2020 9:23 AM UTC

As I have said, memory mapped mode is read-only, you can't directly write values into the array, but you can read them like that as long as you set up memory-mapped mode again after each write access.