Skip to main content
Associate III
May 6, 2025
Question

Is it possible to drive peripheral devices with octospi?

In my design, I want to drive  a dac with octospi.

I need to transmit data via the interface in DAC data frame without any instruction and address.

like:

 *(__IO uint8_t*)&OCTOSPI1->DR = data[i];

 

void OCTOSPI1_Init(void)
{
 OCTOSPI1->CR &= ~OCTOSPI_CR_EN;
 while ((OCTOSPI1->CR & OCTOSPI_CR_EN) != 0);

 OCTOSPI1->DCR1 = (0 << OCTOSPI_DCR1_CSHT_Pos) | (2 << OCTOSPI_DCR1_DEVSIZE_Pos);

 OCTOSPI1->CCR = (0b11 << OCTOSPI_CCR_DMODE_Pos); // Data on 4 lines

 OCTOSPI1->DCR2 = 3;		// prescaler = 4

 OCTOSPI1->DLR = 2; 		// 2

 OCTOSPI1->CR |= OCTOSPI_CR_EN;

 MODIFY_REG(OCTOSPI1->CR, OCTOSPI_CR_FMODE, 0x00000000);
}

void OCTOSPI1_WriteData(uint8_t* data, uint32_t length)
{
 for (uint32_t i = 0; i < length; i++) {
 while (!(OCTOSPI1->SR & OCTOSPI_SR_FTF)); // wait for FIFO available
 *(__IO uint8_t*)&OCTOSPI1->DR = data[i];
 }

 // wait for transmission completion
 while (!(OCTOSPI1->SR & OCTOSPI_SR_TCF));
 OCTOSPI1->FCR |= OCTOSPI_FCR_CTCF; // clear transmission completion flag
}

The operation above will block the mcu totally.

Is it possible to do that by octospi and how to configure?

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
May 6, 2025

I suspect you can do that, the different phases are more of a HAL manifestation. Check library source vs references manual 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
dh_leslieAuthor
Associate III
May 6, 2025

it’ better to know how the hardware works. Only to read the reference manual doesn’t help, and going through various register combinations is also impossible.