Skip to main content
YROSS
Associate
December 18, 2018
Question

Is it possible to copy the code stored in the internal or external flash to the internal SRAM and execute it from SRAM ?

  • December 18, 2018
  • 3 replies
  • 1015 views

..

This topic has been closed for replies.

3 replies

adrian
Associate III
December 18, 2018

You’d need to check out how you declare functions/files to run from the ram with your compiler. It will be linked to a specific RAM address and the startup code will copy it to the correct place in ram from the flash.

Tesla DeLorean
Guru
December 18, 2018

One would need to be aware of whether the code is free standing or has dependencies outside itself. But in the general sense I can copy code to RAM and run it there.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
S.Ma
Principal
December 23, 2018

The linker should generate the code where it would ultimately be placed.

This would bring best performance benefits when having both interrupt vectors and ISR functions in SRAM to prevent ART accelerator jumps in Flash.

When the core has code cache memory, external serial memories performance is much improved.