Skip to main content
RMele
Associate
October 25, 2018
Question

Is it possible to connect the exposed pad to Vss in a VFQFPN36 STM32F103T8U?

  • October 25, 2018
  • 5 replies
  • 1302 views

It's possible connect the exposed pad to Vss in a VFQFPN36 STM32F103T8U? What happen if I do it?

In the datasheet STM say about UFQFPN48 "It is recommended to connect it to VSS", but say nothing about about the VFQFPN36 package

This topic has been closed for replies.

5 replies

Uwe Bonnes
Chief
October 26, 2018

This is clearly missing from the datasheet. I guess, the exposed pin on VFQFPN36 will behave like on UFQFPN48, but some feedback from ST would clear up things.

T J
Senior III
October 26, 2018

if you could check the ePad with a multimeter to the ground pin on the processor...

either way, connected or not...

Yes , you can connect the ePad to Gnd.

provisos:

IMHO

not an ST employee

please check it works, before you make many units...

RMele
RMeleAuthor
Associate
November 7, 2018

​Thank you TJ!

Amel NASRI
ST Technical Moderator
November 6, 2018

Hello,

Sorry for the delay to answer your request.

I confirm that it is recommended to connect the exposed pad of VFQFPN36 STM32F103T8U to VSS.

A note will be added to the relevant datasheet to bring more precision (wait for next revision of the document to add it).

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
RMele
RMeleAuthor
Associate
November 7, 2018

​Thank you Amel!!!. I have 300 boards with the exposed pad connected to Vss, and I was fear to go into production.