Skip to main content
tomasz23
Associate
January 5, 2008
Question

Is it possible co leave Vref+ pin unpowered in Standby ?

  • January 5, 2008
  • 2 replies
  • 645 views
Posted on January 05, 2008 at 16:58

Is it possible co leave Vref+ pin unpowered in Standby ?

    This topic has been closed for replies.

    2 replies

    asterix
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:20

    Hi,

    According to AN2629 : STM32F101xx and STM32F103xx low-power modes and the Reference Manual, It seems that Vref is only available in 100 pins package . In smaller packages, this Power supply ref is bounded internally to VDDA. So, in my understanding you should left it not powered in standby ( where all blocks are Powered off except the VBAT domain)without risks of leakage current, I assume that ST has a good analog design in their rails powers and I/O ring in Low power.

    You can try it at your end and inform me if you observe additional leaks.

    Magigimix ;)

    tomasz23
    tomasz23Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:20

    Hello

    I'm going to use STM32 Standby mode (Vdd & Vdda = 3V from battery)

    but ADC will be working only in Run mode, when main supply (3.3V) will be operating and then Vref+ pin will be powered through LM431C reference

    at the level of 2,5V. But when main supply will be switched off then conseqently Vref+ will be left unpowered ... I cannot supply Vref+ directly from

    Vdda because of 2,5V reference requirement. I do not want to do any ADC conwersions when main supply is not working.

    The question is:

    Is it a safe / possible solution ? Can be Vref+ left unpowered (but connected to LM431C) in Standby ?

    I'm afraid of possible current leaks from Vdd/Vdda to Vref+ in this situation.