Skip to main content
Anitha
Associate III
March 12, 2021
Question

Is it necessary to test both IWDG and WWDG for IEC 60335-1 class B compliance?

  • March 12, 2021
  • 0 replies
  • 552 views

The ST self-test library(en.x-cube-classb-v2-3-0) tested both watchdogs( IWDG and WWDG). Is it necessary to test both IWDG and WWDG for class B compliance? In the self-test library, they used both watchdogs. If I use one watchdog timer let's say WWDG then Do I need to test other one(IWDG) for class B compliance?

This topic has been closed for replies.