Skip to main content
VViro.1
Associate
Jun 22, 2020 10:16 AM UTC
Question

Is dual bank flash configuration available for STM32H743xxxx?

In STM32F7 dual/single bank configuration is available. It can be done using nDBANK bit of FLASH_OPTCR register. 

Ref link: https://www.st.com/resource/en/application_note/dm00266999-stm32f7-series-flash-memory-dual-bank-mode-stmicroelectronics.pdf

For STM32H7, FLASH_OPTCR register is not having nDBANK bit. So, is there any way to use flash with single bank mode for STM32H7?

This topic has been closed for replies.

4 replies

TDK
Jun 22, 2020 11:37 AM UTC

No, the STM32H7 is always in dual bank mode. But this is just an organizational thing. It shouldn't prevent you from using the flash however you want.

"If you feel a post has answered your question, please click ""Accept as Solution""."
VViro.1
VViro.1Author
Associate
Jun 22, 2020 11:55 AM UTC

@TDK​  Thanks for the reply, but will it allow to create (and execute) a single binary having size > 1MB?

TDK
Jun 22, 2020 12:06 PM UTC

Yes. It's still contiguous memory. No issue with that. Just define it as a single section in your linker file with capacity 2MB.

"If you feel a post has answered your question, please click ""Accept as Solution""."
berendi
Principal
Jun 22, 2020 12:40 PM UTC

For the sake of completeness,

STM32H743xI has 2 banks of 1 MByte each forming a contiguous flash memory area, so there would be no issues with a single binary spanning both banks.

STM32H743xG has 2 banks of 512 kByte each mapped to non-contiguous addresses, there is a 512 kByte hole between the two banks.