Skip to main content
jlchoobs
Associate III
May 28, 2012
Question

Is Code Sourcery worth the effort ?

  • May 28, 2012
  • 14 replies
  • 1908 views
Posted on May 28, 2012 at 18:28

I have been using the Atollic (Lite) for my development.

My Atollic Projects work great (doing USB & MMC work).

But I have run out of space with the 32K limit.

So I moved over recently to the Code Sourcery - or tried.

I can compile a simple: main(){while(1){}} program , etc.

But when I try to move and compile my Atollic Projects,

they do not compile.

Simply:

  make -k all

 - with no file outputs, warnings, errors, etc.

I have been using Eclipse WinArm for Atmel for years.

I followed most specs that I could find - on installing Code Sourcery on Eclipse,

 - but with no result.

Is Code Sourcery supposed to work like a Black Box ?

Is there some Verbose parameter needed or something ?

- Any Advice ?

- Does anybody actually promote Code Sourcery ?
    This topic has been closed for replies.

    14 replies

    jlchoobs
    jlchoobsAuthor
    Associate III
    June 7, 2012
    Posted on June 07, 2012 at 16:01

    .. Your FINALLY learning fm ..

    So, can you keep off my other Topics also - until you learn to Respect this Golden Rule - and stop dumping Your Wasteful Negativity on all my posts ?

    I think others also reading this - don't want to hear you either - you provide nothing Useful - only rhetoric ...

    By the way - what don't You Understand about the Words : 'Go Away' - ?

    - You still don't get the idea ...

    frankmeyer9
    Associate III
    June 8, 2012
    Posted on June 08, 2012 at 16:42

    That Golden rule is: ''don't feed the troll''.

    Andrew Neil
    Super User
    June 9, 2012
    Posted on June 09, 2012 at 15:35

    ''This is a Public Forum''

     

     

    Indeed it is - so you don't get to choose who may contribute!

    Ever heard the expression, ''beggars can't be choosers''...?

    ''if you can't provide Free Advice - then Go Away !''

    I am happy to refund double the price you paid for my advice...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    June 9, 2012
    Posted on June 09, 2012 at 15:42

    ''ARE YOU A SALESMAN for Code Sourcery ?''

     

     

    Just for the record, no - I'm not.

    Why do you find it an insult when someone simply points out to you that support options are available?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.