IR communication echo removal through turning interrupt on and off
I am developing IR half duplex communication between two stm32f030 MCU, in the USART section, it is working as full duplex. i want that, whenever i receive anything from first usart, it is then sent to second usart. And to remove echo i want to turn off the usart receiving interrupt and turn it on as soon as it the data is sent to other usart. but the problem is when i do that, Echo is still received please give me any useful solution, i am attaching my code.
void USART2_IRQHandler(void)
{ USART_ITConfig(USART2, USART_IT_RXNE, DISABLE);if( USART_GetITStatus(USART2, USART_IT_RXNE) ){char t = USART2->RDR; // the character from the USART1 data register is saved in t
USART_SendData(USART1,t);USART_ITConfig(USART2, USART_IT_RXNE, ENABLE);
}
void USART1_IRQHandler(void)
{ USART_ITConfig(USART1, USART_IT_RXNE, DISABLE);if( USART_GetITStatus(USART1, USART_IT_RXNE) ){char t = USART1->RDR; // the character from the USART1 data register is saved in t
USART_SendData(USART2,t);USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);
}
#usart #stm32f0