Skip to main content
per3
Associate III
January 30, 2008
Question

interupts

Posted on January 30, 2008 at 17:00

interupts

    This topic has been closed for replies.

    6 replies

    joseph239955
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:22

    With Cortex-M3, interrupt service routines does not need special ''return from interrupt'' instruction. Exception/Interrupt return is triggered if the return instruction put a special value (called EXC_RETURN) to the program counter. This special value is written to LR(R14) by hardware automatically as the processor enter the exception/interrupt handler. As a result, interrupt/exception handlers can be written as normal C functions.

    smart
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:22

    Take a look at stm32f10x_vector.c file and this file is compiler dependent.

    Inside this file you can find out the interrupt vector table for a Cortex M3 where all interrupts functions are defined.

    I hope this will help you to understand.

    per3
    per3Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:22

    I have ride 7, and with it a load of examples came.

    I have successfully tried my own example with EXTI1_IRQHandler.

    To get it to work, one has to call EXTI_init, set EXTI1_IRQChannel with NVIC_Init.

    Since I got it to work, I am happy. However, I would like to understand how the compliler knows that EXTI1_IRQHandler is the interupt routine. I have looked all over and that handler is only defined in stm32f10x_it.c and stm32f10x_it.h. How does this routine get called, and how does the complier know it has to end with a return from interupt?

    joseph239955
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:22

    You can find descriptions of EXC_RETURN in ARM documentation

    Cortex-M3 Technical Reference Manual r1p1 (TRM) section 5.4 and 5.8.

    (http://infocenter.arm.com/)

    ARM v7M Architecture Application Level Reference Manual

    section B1.2.3

    (http://www.arm.com/products/CPUs/ARM_Cortex-M3_v7.html)

    smart
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:22

    Hello Joseph

    Thanks for your reply. That makes perfect sense.

    Where we can find out some more details about EXC_RETURN or return from

    Exc/int in cortex M3.

    :)

    per3
    per3Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:22

    Quote:

    On 28-01-2008 at 18:27, Anonymous wrote:

    Take a look at stm32f10x_vector.c file and this file is compiler dependent.

    Inside this file you can find out the interrupt vector table for a Cortex M3 where all interrupts functions are defined.

    I hope this will help you to understand.

    Thanks, only on the Ride 7 system this file is renamed to crt0_STM32x.c, however in the header comments of this file the file says its name is stm32f10x_vector.c.