Skip to main content
dk2
Associate
October 30, 2009
Question

Interrupts lost while interrupts are disabled

  • October 30, 2009
  • 1 reply
  • 529 views
Posted on October 30, 2009 at 04:14

Interrupts lost while interrupts are disabled

    This topic has been closed for replies.

    1 reply

    dk2
    dk2Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:28

    Hi,

    in my program, the Systick-interrupt sets an external

    interrupt request in the EXTI-SWIER. When this is done, while the

    corresponding bit in the EXTI-IMR is set, everything is ok.

    But when:

    - the main routine disables this int by clearing the IMR-bit

    - with the cleared IMR-bit the SWIER-bit is set (by the still enabled

    Systick-int with high priority)

    - the main routine reenables the int

    then the SWIER bit remains set, but no pending request is set and no int

    is generated.

    It looks like the SWIER is ANDED with the IMR, in contrast to the

    block diagram in RM0008 (June 2009-Version), 9.2.2- Figure 20.

    But even then there should be an interrupt when SWIER and IMR - bits

    are set, regardless of the sequence of their settings. Right?

    Even more, it is said that the PendingRequestRegister must be cleard by

    software by writing a 1 to the bit. But this is done by hardware at the

    start of the interrupt service routine. At the same time the SWIER-Bit

    is automatically cleared. So, no action has to be taken in software.

    (That's what I found out).

    Detlef